|
MSP Graphics Library
|
Functions | |
| void | Graphics_drawRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect) |
| void | Graphics_fillRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect) |
| int32_t | Graphics_isRectangleOverlap (Graphics_Rectangle *rect1, Graphics_Rectangle *rect2) |
| int32_t | Graphics_getRectangleIntersection (Graphics_Rectangle *rect1, Graphics_Rectangle *rect2, Graphics_Rectangle *intersect) |
| bool | Graphics_isPointWithinRectangle (const Graphics_Rectangle *rect, uint16_t x, uint16_t y) |
| void Graphics_drawRectangle | ( | const Graphics_Context * | context, |
| const Graphics_Rectangle * | rect | ||
| ) |
Draws a rectangle.
| context | is a pointer to the drawing context to use. |
| rect | is a pointer to the structure containing the extents of the rectangle. |
This function draws a rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive.
| void Graphics_fillRectangle | ( | const Graphics_Context * | context, |
| const Graphics_Rectangle * | rect | ||
| ) |
Draws a filled rectangle.
| context | is a pointer to the drawing context to use. |
| rect | is a pointer to the structure containing the extents of the rectangle. |
This function draws a filled rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive. The clipping of the rectangle to the clipping rectangle is performed within this routine; the display driver's rectangle fill routine is used to perform the actual rectangle fill.
| int32_t Graphics_getRectangleIntersection | ( | Graphics_Rectangle * | rect1, |
| Graphics_Rectangle * | rect2, | ||
| Graphics_Rectangle * | intersect | ||
| ) |
Determines the intersection of two rectangles.
| rect1 | is a pointer to the first rectangle. |
| rect2 | is a pointer to the second rectangle. |
| intersect | is a pointer to a rectangle which will be written with the intersection of rect1 and rect2. |
This function determines if two rectangles overlap and, if they do, calculates the rectangle representing their intersection. If the rectangles do not overlap, 0 is returned and intersect is not written.
| bool Graphics_isPointWithinRectangle | ( | const Graphics_Rectangle * | rect, |
| uint16_t | x, | ||
| uint16_t | y | ||
| ) |
Determines if a point lies within a given rectangle.
| rect | is a pointer to the rectangle which the point is to be checked against. |
| x | is the X coordinate of the point to be checked. |
| y | is the Y coordinate of the point to be checked. |
This function determines whether point (x, y) lies within the rectangle described by rect.
| int32_t Graphics_isRectangleOverlap | ( | Graphics_Rectangle * | rect1, |
| Graphics_Rectangle * | rect2 | ||
| ) |
Determines if two rectangles overlap.
| rect1 | is a pointer to the first rectangle. |
| rect2 | is a pointer to the second rectangle. |
This function determines whether two rectangles overlap. It assumes that rectangles rect1 and rect2 are valid with xMin < xMax and yMin < yMax.