Logo
Developing with ZBOSS for Zigbee
SE security subsystem

Functions

zb_ret_t zb_se_load_ecc_cert (zb_uint16_t suite, zb_uint8_t *ca_public_key, zb_uint8_t *certificate, zb_uint8_t *private_key)
 Loads device's certificate to NVRAM. More...
 
zb_ret_t zb_se_erase_ecc_cert (zb_uint8_t suite_no, zb_uint8_t *issuer, zb_uint8_t *subject)
 Erases device's certificate from NVRAM. More...
 
zb_bool_t zb_se_has_valid_key (zb_uint16_t addr)
 Checks availability of valid keypair for this device. More...
 
zb_bool_t zb_se_has_valid_key_by_ieee (zb_ieee_addr_t addr)
 
zb_ret_t zb_se_debug_get_link_key (zb_uint16_t addr, zb_uint8_t link_key[ZB_CCM_KEY_SIZE])
 
zb_ret_t zb_se_debug_get_link_key_by_long (zb_ieee_addr_t ieee, zb_uint8_t link_key[ZB_CCM_KEY_SIZE])
 
zb_ret_t zb_se_debug_get_nwk_key (zb_uint8_t key[ZB_CCM_KEY_SIZE])
 
zb_ret_t zb_se_debug_get_ic_key (zb_uint8_t key[ZB_CCM_KEY_SIZE])
 
void zb_se_start_aps_key_establishment (zb_uint8_t param, zb_uint16_t addr)
 Starts procedure of partner APS Link key establishment with specified device. More...
 

Detailed Description

Function Documentation

§ zb_se_debug_get_ic_key()

zb_ret_t zb_se_debug_get_ic_key ( zb_uint8_t  key[ZB_CCM_KEY_SIZE])

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Get APS key generated from the current installcode. To be used mainly for debug purposes.

Parameters
key- buffer for the key
Returns
RET_OK or error code

§ zb_se_debug_get_link_key()

zb_ret_t zb_se_debug_get_link_key ( zb_uint16_t  addr,
zb_uint8_t  link_key[ZB_CCM_KEY_SIZE] 
)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Get APS link key or TCLK for remote device. To be used mainly for debug purposes. Check key availability using zb_se_has_valid_key() before this call.

Parameters
addr- short address of remote device
link_key- buffer for the key
Returns
RET_OK or error code

§ zb_se_debug_get_link_key_by_long()

zb_ret_t zb_se_debug_get_link_key_by_long ( zb_ieee_addr_t  ieee,
zb_uint8_t  link_key[ZB_CCM_KEY_SIZE] 
)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Get APS link key or TCLK for remote device by its long address. To be used mainly for debug purposes.

Parameters
ieee- long address of remote device
link_key- buffer for the key
Returns
RET_OK or error code

§ zb_se_debug_get_nwk_key()

zb_ret_t zb_se_debug_get_nwk_key ( zb_uint8_t  key[ZB_CCM_KEY_SIZE])

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Get current NWK key, To be used mainly for debug purposes.

Parameters
key- buffer for the key
Returns
RET_OK or error code

§ zb_se_erase_ecc_cert()

zb_uint8_t zb_se_erase_ecc_cert ( zb_uint8_t  suite_no,
zb_uint8_t issuer,
zb_uint8_t subject 
)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Erases device's certificate from NVRAM.

Parameters
[in]suite_no- CryptoSuite #
[in]issuer- buffer with certificate's issuer
[in]subject- buffer MAC address (IEEE 802.15.4)
Note
This function is designed mainly for Trust Center devices as for purpose of erasing certificates from NVRAM by suite, issuer and subject(MAC address).

§ zb_se_has_valid_key()

zb_bool_t zb_se_has_valid_key ( zb_uint16_t  addr)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Checks availability of valid keypair for this device.

Parameters
[in]addr- short address of the remote device
Returns
ZB_TRUE if valid key exists, ZB_FALSE otherwise.

Valid key is either TCLK to TC established by CBKE procedure or partner APS Link key established using partner link keys establishment procedure.

Example
if (dev_addr != 0 && !zb_se_has_valid_key(dev_addr)
{
ZB_SCHEDULE_CALLBACK2(zb_se_start_aps_key_establishment, param, dev_addr);
}
See also
zb_se_start_aps_key_establishment - start APS partner link key establishment

§ zb_se_has_valid_key_by_ieee()

§ zb_se_load_ecc_cert()

zb_uint8_t zb_se_load_ecc_cert ( zb_uint16_t  suite,
zb_uint8_t ca_public_key,
zb_uint8_t certificate,
zb_uint8_t private_key 
)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Loads device's certificate to NVRAM.

Parameters
[in]suite- CryptoSuite ID (kec_key_suite)
[in]ca_public_key- buffer with Certification Authority's public key
[in]certificate- buffer with device's certificate
[in]private_key- buffer with device's private key
Note
This function is designed mainly for Trust Center devices as an additional method of adding certificates from several CAs.
Example
#ifdef SE_CRYPTOSUITE_1
zb_se_load_ecc_cert(KEC_CS1, ca_public_key_cs1, esi_certificate_cs1, esi_private_key_cs1);
#endif
#ifdef SE_CRYPTOSUITE_2
zb_se_load_ecc_cert(KEC_CS2, ca_public_key_cs2, esi_certificate_cs2, esi_private_key_cs2);
#endif
See also
zb_se_retry_cbke_with_tc
ZB_SE_SIGNAL_CBKE_FAILED

§ zb_se_start_aps_key_establishment()

void zb_se_start_aps_key_establishment ( zb_uint8_t  param,
zb_uint16_t  addr 
)

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_se.h>

Starts procedure of partner APS Link key establishment with specified device.

Parameters
[in]param- reference to the buffer which will be used for outgoing Match Descriptor Request command
[in]addr- short address of the remote device

ZBOSS indicates completion status of this procedure by passing ZB_SE_SIGNAL_APS_KEY_READY and ZB_SE_SIGNAL_APS_KEY_FAIL signals to the application's signal handler. Application should process this signals if needed.

See also
ZB_SE_SIGNAL_APS_KEY_READY - signal description
ZB_SE_SIGNAL_APS_KEY_FAIL - signal description
ZB_SE_SIGNAL_CBKE_OK - example code of signal handling
zb_se_has_valid_key - check if there is a valid APS key with the device