Radio Control Layer (RCL) 9.20.01.03 Release Notes

Table of Contents

Introduction

The Radio Control Layer (RCL) component for the LPF3 SDK consists of:

Disclaimer

See Upgrade and Compatibility Information for details.

Documentation

The following documentation is included in RCL.

Build Size

The following is the output of the TI ARM Clang size tool:

Component Flash Size (Bytes) RAM Size (Bytes)
LRF 5131 38
RCL 5593 5
HAL 1184 137
ADC Noise Command Handler 870 0
BLE5 Command Handler 20858 0
Generic PHY Command Handler 4806 0
IEEE 802.15.4 Command Handler 8044 0
Totals 46486 (8.87%) 180 (0.49%)

Note this is the total size of the archive, not necessarily the size of the final linked program.

Dependencies

Hardware Setup

This release is tested with the following hardware:

No hardware modifications are required.

What’s New

This list contains all new features in: v9.20

ID Summary
RCL-1012 DMM: Declare RCL_AdcNoise* API as ‘weak’ to enable application specific override
RCL-817 RCL: Update HAL function names with RCL namespace to avoid conflicting symbol names
RCL-389 RCL: Support for Rx window optimization through PHY-specific command start constants
RCL-904 BLE Coex: Support for three-wire mode
RCL-903 BLE Coex: Support for one-wire mode
RCL-710 IEEE 802.15.4: Support for source matching on incoming packets with extended source address
RCL-220 IEEE 802.15.4: Support Dual PAN
RCL-873 BLE: Support PAwR Advertiser
RCL-1286 NESB: Add support for CC27XX
RCL-1351 BLE CS: Tune step timing and PLL performance on CC2340R53 to meet Bluetooth CS PHY qualification test criteria
RCL-1371 BLE CS: Add support for CC2745R10_CS_EVM

Fixed Issues

This list contains all bugfixes in: v9.20

ID Summary
RCL-1258 NESB: PRX command will not respond to graceful stop at certain times
RCL-1263 NESB: Packet payload may be corrupted if a graceful stop is issued during packet reception
RCL-935 BLE: TX output power values not present in the power table are not rounded up as Bluetooth Core Spec requires
RCL-1087 BLE: PAwR Scanner accepts connection request when a connection has already been established
RCL-1347 BLE: Use of long critical sections between the sending of primary advertising packets can cause delayed handling of RCL events potentially leading to radio blackout periods

Known Issues

ID Summary
RCL-343 NESB: Address mismatch counter not implemented

Upgrade and Compatibility Information

HAL Function Names with Namespace

The RCL HAL function and symbol names have been updated from a naming format hal_what_to_do to RCL_Hal_whatToDo. The namespace is introduced to avoid any symbol name overlap across modules. The table below lists previous vs. new symbol names.

Previous Name New Name
hal_init_fsm RCL_Hal_initFsm
hal_trigger_command_fsm RCL_Hal_triggerCommandFsm
hal_trigger_dispatch_fsm RCL_Hal_triggerDispatchFsm
hal_trigger_scheduler_fsm RCL_Hal_triggerSchedulerFsm
hal_get_command_ifg_reg RCL_Hal_getCommandIfgReg
hal_get_dispatch_ifg_reg RCL_Hal_getDispatchIfgReg
hal_get_current_time RCL_Hal_getCurrentTime
hal_enable_setup_time_irq RCL_Hal_enableSetupTimeIrq
hal_setup_setup_time RCL_Hal_setupSetupTime
hal_setup_start_time RCL_Hal_setupStartTime
hal_setup_packet_timeout RCL_Hal_setupPacketTimeout
hal_setup_hard_stop_time RCL_Hal_setupHardStopTime
hal_enable_hard_stop_time_irq RCL_Hal_enableHardStopTimeIrq
hal_disable_hard_stop_time_irq RCL_Hal_disableHardStopTimeIrq
hal_setup_graceful_stop_time RCL_Hal_setupGracefulStopTime
hal_enable_graceful_stop_time_irq RCL_Hal_enableGracefulStopTimeIrq
hal_cancel_setup_time RCL_Hal_cancelSetupTime
hal_cancel_start_time RCL_Hal_cancelStartTime
hal_cancel_packet_timeout RCL_Hal_cancelPacketTimeout
hal_cancel_hard_stop_time RCL_Hal_cancelHardStopTime
hal_cancel_graceful_stop_time RCL_Hal_cancelGracefulStopTime
hal_init_dispatch_radio_interrupts RCL_Hal_initDispatchRadioInterrupts
hal_enable_command_radio_interrupt RCL_Hal_enableCommandRadioInterrupt
hal_disable_command_radio_interrupt RCL_Hal_disableCommandRadioInterrupt
hal_clear_command_radio_interrupt RCL_Hal_clearCommandRadioInterrupt
hal_disable_all_command_radio_interrupts RCL_Hal_disableAllCommandRadioInterrupts
hal_disable_all_dispatch_radio_interrupts RCL_Hal_disableAllDispatchRadioInterrupts
hal_temperature_init RCL_Hal_temperatureInit
hal_get_temperature RCL_Hal_getTemperature
hal_get_vdds_voltage RCL_Hal_getVddsVoltage
hal_get_hfxt_ratio RCL_Hal_getHfxtRatio
hal_get_hfxt_ratio_default RCL_Hal_getHfxtRatioDefault
hal_check_clear_timer_compare RCL_Hal_checkClearTimerCompare
hal_setup_cmd_start_cap RCL_Hal_setupCmdStartCap
hal_arm_cmd_start_cap RCL_Hal_armCmdStartCap
hal_get_cmd_start_cap RCL_Hal_getCmdStartCap
hal_setup_sync_found_cap RCL_Hal_setupSyncFoundCap
hal_arm_sync_found_cap RCL_Hal_armSyncFoundCap
hal_get_sync_found_cap RCL_Hal_getSyncFoundCap
hal_setup_cmd_done_cap RCL_Hal_setupCmdDoneCap
hal_arm_cmd_done_cap RCL_Hal_armCmdDoneCap
hal_get_cmd_done_cap RCL_Hal_getCmdDoneCap
hal_set_rcl_clock_enable RCL_Hal_setRclClockEnable
hal_clear_rcl_clock_enable RCL_Hal_clearRclClockEnable
hal_set_dcdc_ipeak_setting RCL_Hal_setDcdcIpeakSetting
hal_enable_clk_buffer RCL_Hal_enableClkBuffer
hal_power_set_standby_constraint RCL_Hal_powerSetStandbyConstraint
hal_power_release_standby_constraint RCL_Hal_powerReleaseStandbyConstraint
hal_power_set_swtcxo_update_constraint RCL_Hal_powerSetSwTcxoUpdateConstraint
hal_power_release_swtcxo_update_constraint RCL_Hal_powerReleaseSwTcxoUpdateConstraint
hal_power_open RCL_Hal_powerOpen
hal_power_close RCL_Hal_powerClose
hal_set_temperature_notification RCL_Hal_setTemperatureNotification
hal_stop_temperature_notification RCL_Hal_stopTemperatureNotification

Known Limitations

The following scenarios have limited test coverage in the RCL module tests:

Versioning

This product’s version follows a version format, MM.mm.pp.bb, where MM is a 2 digit Major number, mm is a 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.