Radio Control Layer (RCL)
Glossary

A unique 32-bit address used for identifying BLE packet boundaries and distinguishing packets from different connections.

A feature in BLE that allows a device to specify a list of trusted peer devices that can connect, enhancing security and reducing unwanted connections.

Additional Controller Advertising Data (ACAD) field in the extended header. The ACAD field contains data from the Advertiser's Controller or data intended for the recipient's Controller. It follows the format of advertising and scan response data. In Periodic Advertising with Responses (PAwR), the Periodic Advertising Response Timing Information is included in the ACAD field of the AUX_ADV_IND PDU.

Specific radio channels used by BLE devices to advertise data to facilitate discovery and connection establishment.

Advertising data (AD) structures, defined in the advertising and scan response data format, form a significant part of the advertising data. The compositions are detailed in the following table:

Fields Length AD Type AD Data
Octets 1 1 Length - 1

Specific type of BLE PDUs used during the advertising process that contain information about the advertising device such as the device's address or the type of device. They can be transmitted either on primary advertising physical channels or on secondary advertising physical channels.

The time between consecutive advertising events, where a device broadcasts its presence to enable discovery by other devices.

Part of an advertising event that provides additional data beyond the primary advertising data sent over a primary advertising channel.

A 3-octets field included in extended advertising packets to indicate that some or all of the advertising data is in a subsequent auxiliary packet. Among other things, it serves as a reference to the starting point of the auxiliary data, enabling scanning devices to efficiently listen to the auxiliary advertising at the correct time.

Channel Index CA Offset Units AUX Offset AUX PHY
(6 bits) (1 bit) (1 bit) (13 bits) (3 bits)

Contains the time from the reference point to the approximate start of the auxiliary packet, where the reference point is the start of the packet containing the AuxPtr field. The value of the Aux Offset is in the unit of time indicated by the Offset Units field (i.e. the offset is determined by multiplying the value by the unit).

Indicates the PHY used to transmit the auxiliary packet.

A unique 48-bit address assigned to each BLE device, used for identification and addressing.

The part of the BLE packet containing control information, specifying the PDU type, packet length, and CRC information.

The device that initiates and controls the connection, determining the timing and communication parameters in a BLE link.

A list of channels a BLE device uses for communication, indicating which channels it can transmit and receive on.

Contains the general-purpose channel index used to transmit the auxiliary packet.

Channel Sounding is a secure, fine-ranging feature that enables true distance awareness between two Bluetooth devices. It enhances the performance of applications and use cases that require highly accurate and secure device positioning, including Bluetooth “Find My,” digital keys, and more.

Contains the clock accuracy of the advertiser that will be used between the packet containing this data and the auxiliary packet. If "0", the advertiser's clock accuracy is between 51 ppm and 500 ppm. If "1", the advertiser's clock accuracy is between 0 ppm and 50 ppm.

Self-contained state machine that takes care of the command parameters, the payload, and the interrupt handling needed during the execution of radio commands.

A period during which data is exchanged between connected BLE devices, consisting of multiple data transmission and reception windows.

The time between two consecutive connection events, defining how often data is exchanged in a BLE connection.

Standardized format for organizing and transmitting additional data alongside advertising packets in extended advertising events.

Extended Header Length AdvMode Extended Header AdvData
(6 bits) (2 bits)(0-63 octets) (0-254 octets)

Channels used for data exchange after a connection is established, with the primary and secondary advertising channels repurposed for this purpose.

Electronic shelf label (ESL) systems have historically relied on proprietary protocols for wireless communication, which presents a potential barrier to global adoption. To address this challenge, leaders from the ESL industry teamed up with the Bluetooth SIG to create a scalable, ultra-low-power, highly secure ESL wireless standard based on Bluetooth technology.

Extended Advertising is a connectionless communication feature that adds new channels and enables devices to transmit larger amounts of data in their advertising packets. It enhances the capabilities of Bluetooth LE advertising broadcast by enabling more efficient broadcasting, improved range, and support for more complex data exchanges.

Variable length header that is present if, and only if, the Extended Header field is non-zero. It is composed of a group of fields that provide information about the type of advertising.

Extended Header Flags Advertiser's Address Target's Address CTE Info AdvData Info AuxPtr SyncInfo TxPower ACAD
(1 octet) (6 octets) (6 octets) (1 octet) (2 octets) (3 octets) (18 octets) (1 octet) (varies)

Collection of flags part of the Extended Header that indicate if an extended header field is present or not. The extended header fields that are present are always in the same order as the flags in the extended header flags. Whether an extended header flag and corresponding extended header field is mandatory, optional, or reserved for future use depends on the Advertising Physical Channel PDU in which the extended header is used.

In the context of BLE, a technique used to switch between 40 different radio frequencies within the 2.4 GHz ISM band to reduce interference and enhance reliability.

LE 2M is a Gaussian Frequency Shift Keying (GFSK) physical layer (PHY) that enables Bluetooth LE devices to achieve data rates up to 2 Mbps.

LE Coded

LE Coded is a Gaussian Frequency Shift Keying (GFSK) physical layer (PHY) that enhances the range and reliability of Bluetooth LE communication by using forward error correction (FEC). This allows devices to maintain stable connections over longer distances, even in challenging RF environments.

Original advertising method defined in the BLE specification. It involves transmitting advertising packets that are limited in data size and typically used for simple device discovery and connection establishment. Legacy advertising packets are sent over primary advertising channels and have a fixed format suitable for basic use cases.

In the context of BLE, the Link Layer defines the several types of packet that are transmitted over the air and the associated air interface protocol. Aspects such as radio channel selection and classification are defined in the link layer specification.

The Radio IP in charge of Low Power Radio communications.

Signals sent from the LRF to the command handlers and the RCL that contain information about radio-specific events.

Protocol-specific firmware used by the LRF.

Indicates the units used by the Aux Offset field. If "0", the units are 30us, if "1", the units are 300 us.

In the context of BLE, the structure of BLE data packets, including preamble, access address, header, and payload.

Stands for Protocol Data Unit which is the basic unit of data exchanged between BLE devices. PDUs contain information such as advertising data, control commands, and user data. Thee packets are used to establish connections, exchange data and manage the communication between BLE devices.

The device that responds to the central and follows the central's timing in a BLE link.

Periodic Advertising allows devices to broadcast advertising packets at scheduled intervals, improving power efficiency. This feature is particularly useful for use cases like location services and asset tracking, where consistent, low-energy transmissions are needed over extended periods.

Periodic Advertising with Responses (PAwR) is a bi-directional connectionless feature that enables devices to periodically broadcast data at scheduled intervals, improving power efficiency. It also allows devices to receive responses to their advertisements, enabling more efficient and interactive communication. PAwR enables very low-power device networks such as electronic shelf labels (ESL), electric vehicle (EV) battery management, and tire pressure monitoring.

Set of register values describing parameters of a specific radio PHY. Meant to be generated via a tool. It's uploaded to the device as binary arrays which are then directly applied to TOPSM registers.

The Physical Layer defines how the radio transmitter/receiver is used to encode and decode digital data for transmission and receipt. It deals with aspects like modulation, frequency hopping, power control, and signal strength. The PHY layer translates the bits generated by the Link Layer into radio waves for wireless communication.

In the context of extended advertising, PHY switching refers to the ability to change the physical layer (PHY) used for transmitting and receiving advertising packets during an extended advertising event. PHY switching allows for improved performance and efficiency by utilizing different radio characteristics (e.g., data rate, range) for different parts of the advertising event, optimizing the connection between the advertiser and scanner based on environmental conditions and power consumption requirements.

A known bit sequence at the start of each packet, aiding in synchronization between devices.

The first three (channels 37, 38 and 39) of the forty BLE channels within the 2.4GHz ISM band. Used for the initial exchange of advertising data.

Physical (layer) Service Data Unit - often (for example in IEEE 802.15.4) used to describe PHY payload in communication protocols. This does not include any synchronization headers, PHY headers of footers. This does include MAC headers or footers and MAC payloads.

An address used to enhance privacy and prevent tracking, periodically changing to reduce traceability.

Signals sent from the RCL to the command handlers (and vice versa) that contain information about the radio operation.

The remaining 37 channels (channels 0 to 36) which are used for additional advertising (extended advertising) or for scanning and connection requests during some BLE procedures.

A field included in extended advertising packets that contains information about periodic advertising synchronization. Scanners will use this information to listen to a periodic advertising event at the correct time, channel, access address and with the correct CRC initialization.

Offset Base Offset Units Offset Adjust RFU Interval ChM SCA AA CRCInit Periodic Event Counter
(13 bits) (1 bit) (1 bit) (13 bits) (2 octets) (37 bits) (3 bits) (4 octets) (3 octets) (2 octets)

The syncPacketWindowOffset value is the time from a reference point to the start of the AUX_SYNC_IND that the SyncInfo field describes.

If the SyncInfo appears in an advertising PDU, the reference point is the start of the packet containing it (i.e. an AUX_ADV_IND). The value of syncPacketWindowOffset is determined by multiplying the value of the Offset Base field by the unit of time indicated by the Offset Units field and then, if the Offset Adjust field is set to 1, adding 2.4576 seconds.

The Offset Units field is set to 0 if the syncPacketWindowOffset is less than 245,700 [us]. The Offset Adjust field shall be set to 0 if the Offset Units field is set to 0 or if the SyncInfo field appears within an advertising PDU.

The packet containing the AUX_SYNC_IND PDU PDU must not start any earlier than syncPacketWindowOffset after the reference point and must start no later than syncPacketWindowOffset plus one Offset unit after the reference point.

Timer running at a resolution of 250 [ns], used by the RCL for all scheduling-related operations.

Additional synchronization information required for Periodic Advertising with Responses (PAwR) trains is included in the ACAD field. The AD type value for this information is 0x32. The fields are detailed in the following table:

Fields RspAA numSubevents subeventInterval responseSlotDelay responseSlotSpacing
Octets 0 - 3 4 5 6 7

The RspAA field shall be set to the Access Address to be used by thePAwR scanner when it transmits a response packet to the PAwR advertiser.

The numSubevents field shall be set to the number of subevents.

The subeventInterval (Periodic Advertising Subevent Interval) field shall be set to the time, in 1.25 ms units, from the start of one subevent to the start of the next subevent.

The responseSlotDelay (Periodic Advertising Response Slot Delay) field shall be set to the time, in 1.25 ms units, from the start of one subevent to the first response slot.

The responseSlotSpacing (Periodic Advertising Response Slot Spacing) shall be set to the time, in 0.125 ms units, from the start of one response slot to the start of the next response slot.