Post-Build Script imgtool

The compiler output requires a post-build step to generate a .bin file that can be used by MCUboot. An MCUboot compatible image tool must be executed called imgtool. It is responsible for adding the MCUBoot image header, managing keys and sign the image. More detailed description is provided on the imgtool documentation page. This tool requires Python3 and is included in the SimpleLink SDK in the folder <simplelink-install-dir>\source\third_party\mcuboot\scripts.

The script can be executed automatically after every build by adding below lines as Post-Build steps in Properties > Build as shown below. This command defines the image version. To update the version number, adjust the string --version 1.0.0.

Listing 18. Post-Build Steps
1${CG_TOOL_ROOT}/bin/tiarmobjcopy ${ProjName}.out --output-target binary ${ProjName}.bin --remove-section=.ccfg
2${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/tools/common/mcuboot/imgtool sign --header-size 0x100 --align 4 --slot-size 0x4C000 --version 1.0.0 --pad-header --key ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/third_party/mcuboot/root-ec-p256.pem ${ProjName}.bin ${ProjName}.bin

Note

--slot-size is used to indicate the size of the primary or secondary in which the image will be flashed. The value used should be the same as defined in flash_map_backend.h

../_images/mcuboot_postscriptsteps-cc23xx.png

Figure 37. Post-Build steps included in CCS properties