SimpleLink™ CC23xx SDK Zigbee User's Guide
1.00.00
  • Introduction to the SimpleLink Low Power F3 SDK
  • Zigbee Quick Start Guide
  • Introduction
  • The CC23xx or CC27xx SDK Platform
  • FreeRTOS (RTOS Kernel) Overview
  • SimpleLink Low Power F3 SDK Overview
  • Developing Zigbee Applications
  • Developing with SDK CC23xx
  • MCUboot Over-the-Air Download (OAD)
  • Debugging
  • Packet Sniffer
  • System Configuration (SysConfig)
    • Get started with SysConfig
    • Configure The Board Files with SysConfig
    • Reserve Peripheral(s)
    • Hardware View
    • Zigbee Configuration
    • Disable SysConfig
  • EnergyTrace User Guide
  • Migration Guide
  • References
SimpleLink™ CC23xx SDK Zigbee User's Guide
  • »
  • System Configuration (SysConfig)

System Configuration (SysConfig)¶

SysConfig is a graphical tool for configuring your project in CCS. To set up SysConfig please see the section Get started with SysConfig.

  • Get started with SysConfig
    • Using Stand-alone SysConfig
    • Using SysConfig with IAR Workbench
    • Using SysConfig as a Plug-In to CCS
    • Viewing SysConfig Output
  • Configure The Board Files with SysConfig
  • Reserve Peripheral(s)
  • Hardware View
  • Zigbee Configuration
    • Open An Example Project
    • Zigbee Settings
    • Adjust Your Application
  • Disable SysConfig
    • Locating Generated Files
    • Copy Generated Files
    • Modifying Compiler/Linker Settings
    • Exclude Generated Files from Build
    • Optional: Exclude .syscfg from build
Previous Next

© Copyright 2005-2024, Texas Instruments.