Comprehensive List of Fixed Issues

This section will provide a comprehensive list of the issues that have been fixed with each release of the SimpleLink Low Power F3 SDK.

Note

For more information regarding new features, fixed issues, or known issues for a specific SDK, please reference the respective Core SDK release notes. These can be found online through the links provided in each section, or within the SDK at: {SDK_INSTALL_DIR}/docs/simplelink_mcu_sdk/release_notes_coresdk_lpf3_x_xx_xx_xx.html

v8x SDKs

8.40.00.61 (December 2024)

ID

Summary

BLE_LOKI-2511

[Multi Connect][Stability] CC2340R53 Coded PHY Links Terminate when Hold More Than 8 Multiple Connections and Switching Connection PHY Between Coded to 1M/2M PHY`s

BLE_LOKI-2500

Scan Response not received from a bonded device after advertising burst

BLE_LOKI-2484

Setting data length to 0 in GapAdv_loadByHandle causes SW to enter hard fault

BLE_LOKI-2472

[Documentation] Incorrect doxygen for HCI_EXT_SetMaxDtmTxPowerDbmCmd and HCI_EXT_SetTxPowerDbmCmd

BLE_LOKI-2459

[Documentation] HCI_LE_EnhancedTxTestCmd and HCI_LE_TransmitterTestCmd incorrectly state that dataLen is between 0 and 37

BLE_LOKI-2417

Advertising Disabled Unexpectedly when using GAP_ADV_ENABLE_OPTIONS_USE_DURATION

BLE_LOKI-2352

Infrequently, peripheral does not send out peripheral security request and gapbondmgr_pair returns 0x1C

BLE_LOKI-2080

Doxygen for HCIEXT_EnhancedModemTestTxCmd() modified to specify a way to modify the TxPower used

BLE_LOKI-1990

GAP_CB_PHY_UPDATE event is not returned for event: GAP_CB_CONN_ESTABLISHED

BLE_LOKI-1661

[SWAT][Dual ADV] Peripheral fails to enable legacy adv set 2 after create connection to adv set 1 if they are using different address types

8.20.00.119 (October 2024)

ID

Summary

BLE_LOKI-1994

GATTServApp_ReadRsp API documentation error.

BLE_LOKI-1910

GapAdv_prepareLoadByHandle may cause memory issues when executed on a NULL pointer

BLE_LOKI-1690

SysConfig BLE menus exposes non-available features

BLE_LOKI-1672

Scanner may report incorrect Tx Power value for advertiser using advertising sets with different Tx Power values

BLE_LOKI-1653

In rare cases, when RPA refresh interval is low, a connection may fail to be established

BLE_LOKI-1649

[Extender Advertisement] When using Coded PHY as secondary, only S=8 will be used regardless of configuration

BLE_LOKI-1644

GAP_UpdateLinkParamReq interface keeps returning bleAlreadyInRequestedMode when requesting parameters update as a peripheral after having requested as a central

BLE_LOKI-1612

[AE] [Initiator] Connection is established with wrong connection parameters when using different PHY’s for Primary & Secondary channels

BLE_LOKI-1584

Memory leak in OADService_setParameter inside oad_service.c

BLE_LOKI-1491

Update Documentation for HW platform for HCI APIs

BLE_LOKI-1339

DTM Testing Packet Errors

BLE_LOKI-1199

[SWAT] GATT_ReadLongCharValue fails after 307 iterations during stress test

BLE_LOKI-935

HCIExt_EnhancedModemHopTestTxCmd returns success, but test does not start

8.10.01.02 (June 2024)

Release notes

ID

Summary

BLE_LOKI-1893

The host_test example fails to build on Linux/MacOS.

BLE_LOKI-1848

When using same value for Scan Window and Scan Interval, the interval size is not accurate.

BLE_LOKI-1578

After multiple GATT data transmissions, a blePending error was return.

8.10.00.55 (May 2024)

Release notes

ID

Summary

BLE_LOKI-1623

Scannable advertiser only responds to single scan request received in advertisement.

BLE_LOKI-1443

Gatt Notifications cannot be received on Central after erasing all bonds.

BLE_LOKI-1353

SysConfig error when altering the advertisement parameters in Broadcaster role.

BLE_LOKI-1352

Target Address not changing when using directed advertising.

BLE_LOKI-1247

[SWAT][Data Stream] Gatt_WriteLongCharValue() calls with size 512 bytes fails when using TI Clang Compiler.

BLE_LOKI-1146

Advertisements with Limited Discoverable Flag not terminating within lim_adv_timeout (180s).

BLE_LOKI-1034

Critical Section order not optimal in ICall_leaveCSImpl & ICall_enterCSImpl functions.

BLE_LOKI-949

BLE stack does not remove the att rsp msg even when the BLE connection is lost.

BLE_LOKI-1161

[PSIRT] Stack generates unexpected RPA during fuzz attack when using speed optimization.

v7x SDKs

7.20.01.10 (October 2023)

Release notes

ID

Summary

BLE_LOKI-768

Device stops responding after multiple connections

7.20.00.29 (August 2023)

Release notes

ID

Summary

BLE_LOKI-848

CC2340R5 basic_ble_oad_offchip_peripheral Link Terminate when start OAD using bTool

BLE_LOKI-756

Tx Power value in advertisements is not updated after the advertisement are started

BLE_LOKI-755

Bonding fails if LTK not updated in the linkDB

BLE_LOKI-754

HCI_EXT_SetTxPowerDbmCmd() does not change txPower on CC23XX device

BLE_LOKI-721

Repeatedly changing connection PHY sometimes causes connection timeout during long-term stability testing

BLE_LOKI-699

[basic_ble_oad_onchip] GATT caching can cause OAD to fail

BLE_LOKI-698

CC2340R5: Canceling ongoing OAD via BTool causes retryOAD to fail

BLE_LOKI-681

[OAD] CC23xx device does not indicate to Android/ iOS device to not cache GATT table

BLE_LOKI-659

[Basic BLE Profiles - CGM] Notifications are not sent after large amount of measurements are added

BLE_LOKI-657

Basic BLE central device uses a peer’s RP address after bonding

BLE_LOKI-656

basic_ble not using SysConfig parameters for scan and connection parameters

BLE_LOKI-640

HCI_LE_ReadRfPathCompCmd and HCI_LE_WriteRFPathCompCmd not supported

BLE_LOKI-639

[Basic Example] Basic Broadcaster Doesn’t Advertise

BLE_LOKI-477

[SysConfig] Disable the display module checkbox is missing.

7.10.00.35 (May 2023)

Release notes

ID

Summary

BLE_LOKI-494

Central failed to establish connectionWL to peer with RPA from white list

BLE_LOKI-436

Basic BLE project with multirole BLE role advertises intermittently

BLE_LOKI-435

[macOS Build] imgtool command not found - build post process step for OAD examples fails

BLE_LOKI-431

TERMINATION_IND sometimes missed when using ADV Interval < 100ms

BLE_LOKI-405

CC2340R5 current consumption increased by ~1uA due to longer duration of ‘IDLE’ state

BLE_LOKI-250

GAP_ADV_EVT_MASK_SCAN_REQ_NOTI is not processed in the controller

BLE_LOKI-225

CC23X0 hangs after calling scan_enable

BLE_AGAMA-4307

[PSIRT-145] Accepts PairConfirmSend with wrong values

BLE_AGAMA-4307

[PSIRT-144] Accepts PairRandomSend before exchanging public key

BLE_AGAMA-4307

[PSIRT-143] BLE secure pairing: Accepts DHKeyCheckSend with all fields zero