![]() |
![]() |
TI BLE5-Stack API Documentation
9.12.00
|
Contains part of the GAP Bond Manager Parameters values. More...
Data Fields | |
uint8_t | authenPairingOnly |
uint8_t | autoSyncAL |
uint8_t | bondFailAction |
uint8_t | bonding |
uint8_t | eccDebugKeys |
uint8_t | eccReGenPolicy |
uint8_t | eraseBondWhileInConn |
uint8_t | ioCap |
uint8_t | KeyDistList |
uint8_t | KeySize |
uint8_t | mitm |
uint8_t | pairMode |
uint8_t | removeLRUBond |
uint8_t | sameIrkAction |
uint8_t | secureConnection |
Contains part of the GAP Bond Manager Parameters values.
uint8_t authenPairingOnly |
uint8_t autoSyncAL |
uint8_t bondFailAction |
uint8_t bonding |
uint8_t eccDebugKeys |
uint8_t eccReGenPolicy |
uint8_t eraseBondWhileInConn |
uint8_t ioCap |
uint8_t KeyDistList |
uint8_t KeySize |
uint8_t mitm |
uint8_t pairMode |
uint8_t removeLRUBond |
uint8_t sameIrkAction |
uint8_t secureConnection |