|
Radio Control Layer (RCL)
|
#include <stdint.h>
Include dependency graph for hal.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Enumerations | |
| enum | HalTimerEvent { HAL_TIMER_EVT_NONE = 0, HAL_TIMER_EVT_SETUP = 1, HAL_TIMER_EVT_START = 2, HAL_TIMER_EVT_GRACEFUL_STOP = 3, HAL_TIMER_EVT_HARD_STOP = 4, HAL_TIMER_EVT_PACKET_TIMEOUT = 5 } |
| enum | RCL_PowerEvent { RCL_POWER_STANDBY_AWAKE = 0, RCL_POWER_XTAL_AVAILABLE = 1, RCL_POWER_STANDBY_ENTER = 2 } |
| enum HalTimerEvent |
| enum RCL_PowerEvent |
| void hal_init_fsm | ( | void(*)(void) | setupFsmCb, |
| void(*)(void) | schedFsmCb, | ||
| void(*)(void) | commandFsmCb | ||
| ) |
References commandHwi, dispatchHwi, halCommandFsmCb, halDispatchFsmCb, halSchedFsmCb, RF_commandHwi(), RF_dispatchHwi(), RF_schedHwi(), and schedHwi.
Referenced by RCL_init().
| void hal_trigger_command_fsm | ( | void | ) |
Referenced by RCL_Scheduler_postEvent().
| void hal_trigger_dispatch_fsm | ( | void | ) |
Referenced by rclCommandHwi().
| void hal_trigger_scheduler_fsm | ( | void | ) |
Referenced by RCL_Command_submit(), RCL_triggerScheduler(), and rclDispatchHwi().
| uint32_t hal_get_command_ifg_reg | ( | void | ) |
Referenced by RCL_Lite_CommandHwi(), and rclCommandHwi().
| uint32_t hal_get_dispatch_ifg_reg | ( | void | ) |
Referenced by rclDispatchHwi().
| uint32_t hal_get_current_time | ( | void | ) |
Referenced by rclSchedulerProcessCmdStartStopTime().
| void hal_enable_setup_time_irq | ( | void | ) |
Referenced by rclPowerNotify().
| void hal_setup_setup_time | ( | uint32_t | setupTime | ) |
References channel2usage, and SYSTIM_CH2_SETUP.
Referenced by RCL_Lite_Command_start(), and rclSchedulerHwi().
| void hal_setup_start_time | ( | uint32_t | startTime | ) |
References channel2usage, and SYSTIM_CH2_START.
Referenced by rclSchedulerProcessCmdStartStopTime().
| void hal_setup_packet_timeout | ( | uint32_t | stopTime | ) |
| void hal_setup_hard_stop_time | ( | uint32_t | stopTime | ) |
References channel2usage, and SYSTIM_CH2_STOP.
Referenced by RCL_Handler_Ieee_setCustomEventTime(), and RCL_Scheduler_setStopTimes().
| void hal_enable_hard_stop_time_irq | ( | void | ) |
Referenced by RCL_Handler_Ieee_setCustomEventTime().
| void hal_disable_hard_stop_time_irq | ( | void | ) |
| void hal_setup_graceful_stop_time | ( | uint32_t | stopTime | ) |
Referenced by RCL_Scheduler_setStopTimes().
| void hal_enable_graceful_stop_time_irq | ( | void | ) |
| void hal_cancel_setup_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
Referenced by RCL_Lite_Command_start(), and RCL_Lite_CommandHwi().
| void hal_cancel_start_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
Referenced by rclCommandHwi().
| void hal_cancel_packet_timeout | ( | void | ) |
| void hal_cancel_hard_stop_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
Referenced by RCL_Handler_Ieee_restoreStopTime(), RCL_Lite_CommandHwi(), RCL_Scheduler_setStopTimes(), rclCommandHwi(), and rclSchedulerCancelStopTime().
| void hal_cancel_graceful_stop_time | ( | void | ) |
Referenced by RCL_Lite_CommandHwi(), RCL_Scheduler_setStopTimes(), rclCommandHwi(), and rclSchedulerCancelStopTime().
| void hal_init_dispatch_radio_interrupts | ( | uint32_t | mask | ) |
Referenced by rclPowerNotify(), and rclSchedulerHwi().
| void hal_enable_command_radio_interrupt | ( | uint32_t | mask | ) |
Referenced by LRF_enableHwInterrupt(), and RCL_Lite_Command_start().
| void hal_disable_command_radio_interrupt | ( | uint32_t | mask | ) |
Referenced by LRF_disableHwInterrupt().
| void hal_clear_command_radio_interrupt | ( | uint32_t | mask | ) |
Referenced by LRF_clearHwInterrupt().
| void hal_disable_all_command_radio_interrupts | ( | void | ) |
Referenced by RCL_Lite_CommandHwi(), and rclCommandHwi().
| void hal_disable_all_dispatch_radio_interrupts | ( | void | ) |
Referenced by rclDispatchHwi().
| void hal_temperature_init | ( | void | ) |
Referenced by RCL_init().
| int16_t hal_get_temperature | ( | void | ) |
| uint16_t hal_get_vdds_voltage | ( | void | ) |
Referenced by __attribute__(), and LRF_applyAntennaSelection().
| uint32_t hal_get_hfxt_ratio | ( | void | ) |
References RCL_DEFAULT_HFTRACKCTL_RATIO.
Referenced by LRF_scaleFreqWithHFXTOffset().
| uint32_t hal_get_hfxt_ratio_default | ( | void | ) |
References RCL_DEFAULT_HFTRACKCTL_RATIO.
Referenced by LRF_scaleFreqWithHFXTOffset().
| HalTimerEvent hal_check_clear_timer_compare | ( | void | ) |
References channel2usage, HAL_TIMER_EVT_GRACEFUL_STOP, HAL_TIMER_EVT_HARD_STOP, HAL_TIMER_EVT_NONE, HAL_TIMER_EVT_SETUP, HAL_TIMER_EVT_START, SYSTIM_CH2_SETUP, SYSTIM_CH2_START, and SYSTIM_CH2_STOP.
Referenced by RCL_Lite_CommandHwi(), and rclCommandHwi().
| void hal_setup_cmd_start_cap | ( | void | ) |
| void hal_arm_cmd_start_cap | ( | void | ) |
| uint32_t hal_get_cmd_start_cap | ( | void | ) |
| void hal_setup_sync_found_cap | ( | void | ) |
| void hal_arm_sync_found_cap | ( | void | ) |
| uint32_t hal_get_sync_found_cap | ( | void | ) |
| void hal_setup_cmd_done_cap | ( | void | ) |
| void hal_arm_cmd_done_cap | ( | void | ) |
| uint32_t hal_get_cmd_done_cap | ( | void | ) |
| void hal_set_rcl_clock_enable | ( | uint16_t | mask | ) |
References CLK_DEP_RCL, and hal_set_clock_enable().
Referenced by LRF_setRclClockEnable().
| void hal_clear_rcl_clock_enable | ( | uint16_t | mask | ) |
References CLK_DEP_RCL, and hal_clear_clock_enable().
Referenced by LRF_clearRclClockEnable().
| uint8_t hal_set_dcdc_ipeak_setting | ( | uint8_t | setting | ) |
References LRF_DEFAULT_DCDC_IPEAK_SETTING.
Referenced by LRF_disable(), and LRF_enable().
| void hal_enable_clk_buffer | ( | void | ) |
Referenced by RCL_open().
| void hal_power_set_standby_constraint | ( | void | ) |
| void hal_power_release_standby_constraint | ( | void | ) |
| void hal_power_set_swtcxo_update_constraint | ( | void | ) |
Referenced by LRF_updateTemperatureCompensation(), RCL_Handler_ADC_Noise_getNoise(), RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_aux_adv(), RCL_Handler_BLE5_ChannelAssessment(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_periodicAdv(), RCL_Handler_BLE5_periodicScan(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_BLE_CS_Precal(), RCL_Handler_Generic_prepareSynth(), RCL_Handler_Ieee_RxTx(), and RCL_Handler_Ieee_TxTest().
| void hal_power_release_swtcxo_update_constraint | ( | void | ) |
Referenced by LRF_updateTemperatureCompensation(), RCL_Handler_ADC_Noise_getNoise(), RCL_Handler_Adc_Noise_powerDown(), RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_aux_adv(), RCL_Handler_BLE5_ChannelAssessment(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_periodicAdv(), RCL_Handler_BLE5_periodicScan(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_BLE_CS_Precal(), RCL_Handler_Generic_setSynthPowerState(), RCL_Handler_Ieee_RxTx(), and RCL_Handler_Ieee_TxTest().
| void hal_power_open | ( | void(*)(RCL_PowerEvent) | rclPowerNotifyFunction | ) |
References hal_power_post_notify_fxn(), powerAwakeStandbyObj, and powerEnterStandbyObj.
Referenced by RCL_openPowerNotifications().
| void hal_power_close | ( | void | ) |
References powerAwakeStandbyObj, and powerEnterStandbyObj.
Referenced by RCL_closePowerNotifications().
| void hal_set_temperature_notification | ( | int16_t | currentTemperature, |
| uint16_t | temperatureRange, | ||
| void(*)(int16_t) | rclTemperatureNotify | ||
| ) |
References hal_temperature_post_notify_fxn(), and temperatureChangeNotifyObj.
Referenced by LRF_enableTemperatureMonitoring().
| void hal_stop_temperature_notification | ( | void | ) |
References temperatureChangeNotifyObj.
Referenced by LRF_disableTemperatureMonitoring().