TI BLE5-Stack API Documentation  9.11.00
Data Fields
gapUpdateLinkParamReqReply_t Struct Reference

Data Fields

uint8_t accepted
 TRUE if host accepts parameter update, FALSE otherwise.
 
uint16_t connectionHandle
 Connection handle of the update.
 
uint16_t connLatency
 Connection Latency.
 
uint16_t connTimeout
 Connection Timeout.
 
uint16_t intervalMax
 Maximum Connection Interval.
 
uint16_t intervalMin
 Minimum Connection Interval.
 
uint8_t signalIdentifier
 L2CAP Signal Identifier.
 

Detailed Description

Update Link Parameters Request Reply parameters

This is used by GAP_UpdateLinkParamReqReply


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale