Logo
Developing with ZBOSS for Zigbee
Add group command definitions

Data Structures

struct  zb_zcl_groups_add_group_req_s
 Add group command structure. More...
 
struct  zb_zcl_groups_add_group_res_s
 Add group response command structure. More...
 

Macros

#define ZB_ZCL_GROUPS_GET_ADD_GROUP_REQ(data_buf, add_group_req)
 Parses Add group command and fills in data request structure. If request contains invalid data, ZB_ZCL_NULL_ID is stored as group_id. More...
 
#define ZB_ZCL_GROUPS_GET_ADD_GROUP_RES(data_buf, add_group_res)
 Parses Add group response command and returns response data structure or NULL if request contains invalid data. More...
 
#define ZB_ZCL_GROUPS_SEND_ADD_GROUP_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, group_id)
 Send Add group command. More...
 

Typedefs

typedef struct zb_zcl_groups_add_group_req_s zb_zcl_groups_add_group_req_t
 Add group command structure. More...
 
typedef struct zb_zcl_groups_add_group_res_s zb_zcl_groups_add_group_res_t
 Add group response command structure. More...
 

Detailed Description

Add group request and response commands have simple payload. Response command is being filled and sent by ZCL internals.

Examples

Filling and sending Add Group request:

Macro Definition Documentation

§ ZB_ZCL_GROUPS_GET_ADD_GROUP_REQ

#define ZB_ZCL_GROUPS_GET_ADD_GROUP_REQ (   data_buf,
  add_group_req 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_groups.h>

Value:
{ \
zb_zcl_groups_add_group_req_t *add_group_req_ptr; \
(add_group_req_ptr) = zb_buf_len(data_buf) >= ZB_ZCL_ADD_GROUP_REQ_SIZE ? \
\
if (add_group_req_ptr) \
{ \
ZB_HTOLE16(&(add_group_req).group_id, &add_group_req_ptr->group_id);\
/* group name currently is not supported - do not check it */ \
} \
else \
{ \
add_group_req.group_id = ZB_ZCL_NULL_ID; \
} \
}
Add group command structure.
Definition: zb_zcl_groups.h:155
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Parses Add group command and fills in data request structure. If request contains invalid data, ZB_ZCL_NULL_ID is stored as group_id.

Parameters
data_buf- pointer to zb_buf_t buffer containing command request data
add_group_req- variable to save command request
Note
data_buf buffer should contain command request payload without ZCL header.

§ ZB_ZCL_GROUPS_GET_ADD_GROUP_RES

#define ZB_ZCL_GROUPS_GET_ADD_GROUP_RES (   data_buf,
  add_group_res 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_groups.h>

Value:
{ \
(add_group_res) = zb_buf_len(data_buf) >= ZB_ZCL_ADD_GROUP_RES_SIZE ? \
\
if (add_group_res) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(add_group_res)->group_id); \
/* group name currently is not supported - do not check it */ \
} \
}
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
Add group response command structure.
Definition: zb_zcl_groups.h:194
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Parses Add group response command and returns response data structure or NULL if request contains invalid data.

Parameters
data_buf- pointer to zb_buf_t buffer containing command response data
add_group_res- out pointer to zb_zcl_groups_add_group_res_t, containing command response record
Note
data_buf buffer should contain response command payload without ZCL header

§ ZB_ZCL_GROUPS_SEND_ADD_GROUP_REQ

#define ZB_ZCL_GROUPS_SEND_ADD_GROUP_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  def_resp,
  cb,
  group_id 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_groups.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, def_resp) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_GROUPS_ADD_GROUP); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (group_id)); \
/* Group name currently is not supported, put empty string */ \
ZB_ZCL_PACKET_PUT_DATA8(ptr, ZB_ZCL_NULL_STRING); \
ZB_ZCL_FINISH_PACKET(buffer, ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, ZB_ZCL_CLUSTER_ID_GROUPS, cb); \
}
#define ZB_ZCL_CLUSTER_ID_GROUPS
Definition: zb_zcl_common.h:211
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1468
Definition: zb_zcl_groups.h:90

Send Add group command.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
def_resp- enable/disable default response
cb- callback for getting command send status
group_id- group ID to add

Typedef Documentation

§ zb_zcl_groups_add_group_req_t

§ zb_zcl_groups_add_group_res_t