|
Radio Control Layer (RCL)
|
#include <ti/drivers/rcl/RCL_Command.h>#include <ti/drivers/rcl/RCL_Buffer.h>#include <ti/drivers/rcl/handlers/ble_cs.h>#include <ti/drivers/utils/List.h>
Include dependency graph for ble_cs.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Data Structures | |
| struct | RCL_CmdBleCs_IQSample |
| BLE Channel Sounding IQ Sample. More... | |
| struct | RCL_CmdBleCs |
| BLE Channel Sounding. More... | |
| struct | RCL_CmdBleCs_Step_Internal |
| BLE Channel Sounding Step. More... | |
| struct | MagnData |
| BLE Channel Sounding QQ data. More... | |
| struct | RCL_CmdBleCs_StepResult_Internal |
| BLE Channel Sounding Step Result. More... | |
| union | S2RSample |
| BLE Channel Sounding S2R Sample type definition. More... | |
| struct | RCL_CmdBleCs_S2r |
| BLE Channel Sounding S2R IQ Data. More... | |
| struct | RCL_CmdBleCs_Stats |
| BLE Channel Sounding Statistics. More... | |
| struct | RCL_CmdBleCs_DCSample |
| BLE Channel Sounding DC Sample. More... | |
| struct | RCL_CmdBleCs_PrecalEntry |
| DC precalibration entry. More... | |
| struct | RCL_CmdBleCs_PrecalTable |
| DC precalibration table. More... | |
| struct | RCL_CmdBleCs_Precal |
| DC precalibration command. More... | |
| struct | RCL_CmdBleCs_Step |
| Container format for a single step in the subevent. More... | |
| struct | RCL_CmdBleCs_SubeventResults |
| Container format for a batch of step results in the subevent (first segment) More... | |
| struct | RCL_CmdBleCs_SubeventResultsContinue |
| Container format for a batch of step results in the subevent (second+ segment) More... | |
| struct | RCL_CmdBleCs_Tone |
| Container format for tones. More... | |
| struct | RCL_CmdBleCs_Result |
| Container format for common section of step results. More... | |
| struct | RCL_CmdBleCs_ResultI0 |
| Container format for mode-0 step results. More... | |
| struct | RCL_CmdBleCs_ResultR0 |
| Container format for mode-0 step results. More... | |
| struct | RCL_CmdBleCs_ResultIR1 |
| Container format for mode-1 step results. More... | |
| struct | RCL_CmdBleCs_ResultIR2 |
| Container format for mode-2 step results. More... | |
| struct | RCL_CmdBleCs_ResultIR3 |
| Container format for mode-3 step results. More... | |
| struct | RCL_CMD_BLE_CS_t.mode |
| struct | RCL_CMD_BLE_CS_t.antennaConfig |
| struct | RCL_CMD_BLE_CS_t.timing |
| struct | RCL_CMD_BLE_CS_t.frontend |
Functions | |
| void | RCL_Handler_BLE_CS_PrecalDefaultCallback (RCL_CmdBleCs_PrecalTable *table, uint8_t channel, RCL_CmdBleCs_IQSample *pHigh, RCL_CmdBleCs_IQSample *pLow) |
| struct RCL_CMD_BLE_CS_SUBEVENT_RESULTS_t | __attribute__ ((packed)) |
Variables | |
| uint8_t | subeventCode |
| uint16_t | connectionHandle |
| uint8_t | configID |
| uint16_t | startAclConnectionEvent |
| uint16_t | procedureCounter |
| int16_t | frequencyCompensation |
| int8_t | referencePowerLevel |
| uint8_t | procedureDoneStatus |
| uint8_t | subeventDoneStatus |
| uint8_t | abortReason |
| uint8_t | numAntennaPath |
| uint8_t | numStepsReported |
| uint8_t | data [] |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_TONE_t | __attribute__ |
| uint8_t | mode |
| uint8_t | channel |
| uint8_t | dataLength |
| struct RCL_CMD_BLE_CS_IQ_SAMPLE_t |
| struct RCL_CMD_BLE_CS_t |
BLE Channel Sounding.
Command to execute a BLE Channel Sounding event
| Data Fields | ||
|---|---|---|
| RCL_Command | common | |
| struct RCL_CMD_BLE_CS_t | mode | |
| struct RCL_CMD_BLE_CS_t | antennaConfig | |
| struct RCL_CMD_BLE_CS_t | timing | |
| struct RCL_CMD_BLE_CS_t | frontend | |
| RCL_CmdBleCs_PrecalTable * | precalTable |
Pointer to a table contains DC values from precalibration |
| RCL_CmdBleCs_StepResult_Internal * | results |
Pointer to result list |
| RCL_CmdBleCs_Stats * | stats |
Pointer to statistics structure |
| List_List | stepBuffers |
Linked list of steps to be executed |
| List_List | stepBuffersDone |
Linked list of steps have been executed |
| List_List | resultBuffers |
Linked list of empty result buffers |
| List_List | resultBuffersDone |
Linked list of result buffers containing data |
| List_List | s2rBuffers |
Linked list of empty s2r containers |
| List_List | s2rBuffersDone |
Linked list of s2r containers with data |
| struct RCL_CMD_BLE_CS_STEP_INTERNAL_t |
BLE Channel Sounding Step.
Descriptor to configure a single step within the BLE Channel Sounding Event
| Data Fields | ||
|---|---|---|
| uint16_t | channelIdx |
Integer index of channel information (0: 2402MHz) |
| uint16_t | mode |
Step mode RCL_CmdBleCs_StepMode |
| uint16_t | toneExtension |
Configuration of tone extension |
| uint16_t | payloadLen |
Length of payload in units of 32bit words RCL_CmdBleCs_Payload |
| uint16_t | foffErr |
Internal! Used for frequency offset compensation |
| uint16_t | tAdjustA |
Internal! Used for timegrid adjustment |
| uint16_t | tAdjustB |
Internal! Used for timegrid adjustment |
| uint16_t | reserved0 | |
| RCL_CmdBleCs_IQSample | dcComp[RCL_BLE_CS_NUM_RX_GAIN_LEVEL] |
Internal! Used for DC compensation with precalibrated values |
| uint32_t | payloadTx[RCL_BLE_CS_MAX_PAYLOAD_SIZE] |
Payload to transmit containing random bit sequence (TX) |
| uint32_t | payloadRx[RCL_BLE_CS_MAX_PAYLOAD_SIZE] |
Expected payload to receive containing random bit sequence (RX) |
| uint32_t | aaTx |
Access Address to be transmitted |
| uint32_t | aaRx |
Access Address to be received |
| uint8_t | antennaPermIdx |
Index of entry to be used from the antenna permutation table RCL_CmdBleCs_AntennaConfig |
| uint8_t | antennaPacket |
Index of physical antenna to be used for all packet exchanges RCL_CMD_BLE_CS_PacketAntenna_e |
| uint16_t | antennaSequence |
Internal! Decoded antenna control sequence based on permutation table |
| uint16_t | tStep |
Internal! The total duration of step dynamically calculated |
| uint16_t | tAntennaA |
Internal! Antenna timing adjustment |
| uint16_t | tAntennaB |
Internal! Antenna timing adjustment |
| uint16_t | reserved1 | |
| struct MagnData |
BLE Channel Sounding QQ data.
Container to store RSSI data for postprocess of the quality of tone
| struct RCL_CMD_BLE_CS_STEP_RESULT_INTERNAL_t |
BLE Channel Sounding Step Result.
Container to store the results of a single step within the BLE Channel Sounding Event
Collaboration diagram for RCL_CmdBleCs_StepResult_Internal:| Data Fields | ||
|---|---|---|
| uint16_t | channelIdx |
Integer index of channel information (0: 2402MHz) |
| uint16_t | mode |
Step mode RCL_CmdBleCs_StepMode |
| uint16_t | toneExtension |
Configuration of tone extension |
| uint16_t | payloadLen |
Length of payload in units of 32bit words RCL_CmdBleCs_Payload |
| uint16_t | reserved | |
| int16_t | foffMeasured |
Frequency offset between devices (only set on Initiator Mode 0) |
| uint16_t | pktResult |
Result of packet reception RCL_CmdBleCs_PacketResult |
| uint8_t | gain |
LNA gain used (Low/High) |
| int8_t | pktRssi |
Receiver Signal Strength Indicator [dBm] captured during packet reception |
| uint16_t | rtt |
RTT timestamp |
| uint16_t | corr[RCL_BLE_CS_NUM_CORR] |
Correlator before-peak-after values for fractional time estimation |
| RCL_CmdBleCs_IQSample | dc |
DC offset measured on packet |
| RCL_CmdBleCs_IQSample | pct[RCL_BLE_CS_MAX_NUM_ANT_PATH] |
Phase Correction Terms per antenna path (incl. extension) |
| uint32_t | payload[RCL_BLE_CS_MAX_PAYLOAD_SIZE] |
Payload containing random bit sequence (RX) |
| MagnData | magn[RCL_BLE_CS_MAX_NUM_ANT_PATH] |
Received magnitude data of tone per antenna path for quality estimation (incl. extension) |
| uint8_t | antennaPermIdx |
Index of entry to be used from the antenna permutation table RCL_CmdBleCs_AntennaConfig |
| uint8_t | antennaPacket |
Index of physical antenna to be used for all packet exchanges RCL_CMD_BLE_CS_PacketAntenna_e |
| uint16_t | reserved1 | |
| union S2RSample |
| struct RCL_CMD_BLE_CS_S2R_t |
BLE Channel Sounding S2R IQ Data.
Container to store raw S2R samples of a BLE Channel Sounding Step
Collaboration diagram for RCL_CmdBleCs_S2r:| Data Fields | ||
|---|---|---|
| uint8_t | idx |
The index of entry in the step list which the data belongs to |
| uint8_t | phy |
Phy the samples captured on |
| uint8_t | channel |
Frequency channel |
| uint8_t | payloadLen |
Payload length in bits |
| uint32_t | payload0 |
Payload bits [00:31] |
| uint32_t | payload1 |
Payload bits [32:63] |
| uint32_t | payload2 |
Payload bits [64:95] |
| uint32_t | payload3 |
Payload bits [96:127] |
| uint16_t | iqLength |
Number of valid iq samples in data[] |
| uint16_t | reserved | |
| S2RSample | data[] |
Raw samples captured |
| struct RCL_CMD_BLE_CS_STATS_t |
BLE Channel Sounding Statistics.
Container to store the statistical outputs of the BLE Channel Sounding Event
| struct RCL_CMD_BLE_CS_DC_SAMPLE_t |
BLE Channel Sounding DC Sample.
Container to store DC information
| struct RCL_CMD_BLE_CS_PRECAL_ENTRY_t |
| struct RCL_CMD_BLE_CS_PRECAL_TABLE_t |
DC precalibration table.
Data structure to store and use the DC precalibration table.
| Data Fields | ||
|---|---|---|
| RCL_CmdBleCs_PrecalCallback | callback | |
| uint32_t | timestamp | |
| uint8_t | highThreshold | |
| uint8_t | lowThreshold | |
| uint8_t | rxGain | |
| int8_t | temperature | |
| uint8_t | chSpacing | |
| uint8_t | numEntries: 7 | |
| uint8_t | valid: 1 | |
| RCL_CmdBleCs_PrecalEntry | entries[] | |
| struct RCL_CMD_BLE_CS_PRECAL_t |
| struct RCL_CMD_BLE_CS_STEP_t |
Container format for a single step in the subevent.
Compressed format used within a multibuffer
| Data Fields | ||
|---|---|---|
| uint32_t | channelIdx: 7 |
Integer index of channel information (0: 2402MHz) |
| uint32_t | mode: 2 |
Step mode RCL_CmdBleCs_StepMode |
| uint32_t | antennaPacket: 3 |
Index of physical antenna for the packet exchange RCL_CMD_BLE_CS_PacketAntenna_e |
| uint32_t | antennaPermIdx: 5 |
Index of entry to be used from the antenna permutation table RCL_CmdBleCs_AntennaConfig |
| uint32_t | toneExtension: 2 |
Enable tone extension, [0]=first tone (transmitted by initiator), [1]=second tone (transmitted by reflector) |
| uint32_t | payloadLen: 3 |
Length of payload in units of 32bit words RCL_CmdBleCs_Payload |
| uint32_t | reserved: 10 | |
| uint32_t | aaTx |
Access Address to be transmitted |
| uint32_t | aaRx |
Access Address to be received |
| uint32_t | payloadTx[RCL_BLE_CS_MAX_PAYLOAD_SIZE] |
Payload to transmit containing random bit sequence (TX) |
| uint32_t | payloadRx[RCL_BLE_CS_MAX_PAYLOAD_SIZE] |
Expected payload to receive containing random bit sequence (RX) |
| struct RCL_CMD_BLE_CS_SUBEVENT_RESULTS_t |
Container format for a batch of step results in the subevent (first segment)
The data[] field contains the results in mode specific format (size varies with step-mode)
| struct RCL_CMD_BLE_CS_SUBEVENT_RESULTS_CONTINUE_t |
Container format for a batch of step results in the subevent (second+ segment)
The data[] field contains the results in mode specific format (size varies with step-mode)
| struct RCL_CMD_BLE_CS_STEP_RESULTS_TONE_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_I0_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_R0_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_IR1_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_IR2_t |
| struct RCL_CMD_BLE_CS_STEP_RESULTS_IR3_t |
| struct RCL_CMD_BLE_CS_t.mode |
| Data Fields | ||
|---|---|---|
| uint16_t | role:2 |
Role of the device RCL_CmdBleCs_Role |
| uint16_t | phy:2 |
Phy used for packet exchange RCL_CmdBleCs_Phy |
| uint16_t | repeatSteps:1 |
Enable continuous repetition of step list |
| uint16_t | chFilterEnable:1 |
Enable filtering of restricted channels at (2402, 2403, 2425, 2426, 2427, 2479, 2480 MHz) |
| uint16_t | precal:1 |
Enable usage of DC precalibration values |
| uint16_t | reportFormat:1 |
Select a vendor specific report format instead of the default HCI LE CS subevent result |
| uint16_t | nSteps:8 |
Total number of steps within the BLE CS Sub-Event |
| struct RCL_CMD_BLE_CS_t.antennaConfig |
| Data Fields | ||
|---|---|---|
| uint8_t | select |
Antenna path configuration by index RCL_CmdBleCs_AntennaConfig |
| uint8_t | gpoMask |
IO mask defining the actively used pins for antenna control |
| uint8_t | gpoVal[RCL_BLE_CS_MAX_NUM_ANT] |
IO value to be used to activate the corresponding antenna ([0]:ANT0, [1]:ANT1, [2]:ANT3, [3]:ANT3) |
| struct RCL_CMD_BLE_CS_t.timing |
| Data Fields | ||
|---|---|---|
| uint16_t | tFcs |
Config of time of Frequency Change period RCL_CmdBleCs_Tfcs |
| uint16_t | tFm |
Config of time of Frequency Measurement period |
| uint16_t | tPm |
Config of time of Phase Measurement Duration RCL_CmdBleCs_Tpm |
| uint16_t | tIp1 |
Config of time of Interlude Period 1 RCL_CmdBleCs_Tip |
| uint16_t | tIp2 |
Config of time of Interlude Period 2 RCL_CmdBleCs_Tip |
| uint16_t | tRxWideningR0 |
Config of additional time of RX timeout of mode-0 steps on reflector. |
| uint16_t | tSw |
Config of time of Antenna Switching duration RCL_CmdBleCs_Tsw |
| uint16_t | tSwAdjustA |
Time adjustment of first set of antenna switching within a step (Pkt-Tn / ...) |
| uint16_t | tSwAdjustB |
Time adjustment of second set of antenna switching within a step (... / Tn-Pkt) |
| struct RCL_CMD_BLE_CS_t.frontend |
| Data Fields | ||
|---|---|---|
| RCL_Command_TxPower | txPower |
Transmit power |
| uint8_t | rxGain |
0: Automatic Gain Control enabled, 1...15: Index value of manual RX gain RCL_CmdBleCs_RxGain |
| int16_t | foffOverride |
Frequency offset compensation override value in [4xFOFF = 4x (FRF/2^21)] units. |
| uint16_t | foffOverrideEnable:1 |
Disables automatic frequency offset estimation and enforces the use of the provided override value |
| uint16_t | reserved:15 | |
| #define RCL_CMDID_BLE_CS 0x1101U |
| #define RCL_CMDID_BLE_CS_PRECAL 0x1102U |
| #define RCL_BLE_CS_US_TO_MCE_TIMER | ( | x | ) | ((x)*48) |
Referenced by RCL_Handler_BLE_CS_preprocessCommand().
| #define RCL_BLE_CS_US_TO_PBE_TIMER | ( | x | ) | ((x)*4) |
| #define RCL_BLE_CS_MCE_TIMER_TO_US | ( | x | ) | ((x)/48) |
| #define RCL_BLE_CS_PBE_TIMER_TO_US | ( | x | ) | ((x)/4) |
| #define RCL_BLE_CS_MCE_TIMER_TO_PBE_TIMER | ( | x | ) | ((x)/12) |
Referenced by RCL_Handler_BLE_CS_preprocessCommand(), and RCL_Handler_BLE_CS_preprocessStep().
| #define RCL_BLE_CS_MAX_NUM_ANT 4 |
| #define RCL_BLE_CS_MAX_NUM_ANT_PATH 5 |
| #define RCL_BLE_CS_MAX_PAYLOAD_SIZE 4 |
Referenced by RCL_Handler_BLE_CS_preprocessStep().
| #define RCL_BLE_CS_NUM_CORR 3 |
| #define RCL_BLE_CS_NUM_STIM 2 |
| #define RCL_BLE_CS_MAX_S2R_LEN 1024 |
Referenced by RCL_Handler_BLE_CS_configureS2R().
| #define RCL_BLE_CS_NUM_RX_GAIN_LEVEL 2 |
| #define RCL_BLE_CS_STEP_RX_GAIN_DB 3 |
Referenced by RCL_Handler_BLE_CS_retrieveAndStoreNextResult().
| #define RCL_BLE_CS_NUM_PRECAL_CHANNELS 8 |
| #define RCL_CmdBleCs_Default | ( | ) |
| #define RCL_CmdBleCs_DefaultRuntime | ( | ) | (RCL_CmdBleCs) RCL_CmdBleCs_Default() |
| #define RCL_CmdBleCs_PrecalTable_Default | ( | ) |
| #define RCL_CmdBleCs_Precal_Default | ( | pTable | ) |
| #define RCL_CmdBleCs_Precal_DefaultRuntime | ( | pTable | ) | (RCL_CmdBleCs_Precal) RCL_CmdBleCs_Precal_Default(pTable) |
| #define RCL_CMD_BLE_CS_FREQCOMP_NA 0xC000 |
| #define RCL_CMD_BLE_CS_TOAD_NA 0x8000 |
Referenced by RCL_Handler_BLE_CS_convertStepResult().
| #define RCL_CMD_BLE_CS_RSSI_NA 0x7F |
| #define RCL_CMD_BLE_CS_SUBEVENT_RESULTS_OPCODE 0x31 |
Referenced by RCL_Handler_BLE_CS_retrieveAndStoreNextResult().
| #define RCL_CMD_BLE_CS_SUBEVENT_RESULTS_CONTINUE_OPCODE 0x32 |
Referenced by RCL_Handler_BLE_CS_retrieveAndStoreNextResult().
| typedef enum RCL_CMD_BLE_CS_Phy_e RCL_CmdBleCs_Phy |
| typedef enum RCL_CMD_BLE_CS_Role_e RCL_CmdBleCs_Role |
| typedef enum RCL_CMD_BLE_CS_StepMode_e RCL_CmdBleCs_StepMode |
| typedef enum RCL_CMD_BLE_CS_PacketResult_e RCL_CmdBleCs_PacketResult |
| typedef enum RCL_CMD_BLE_CS_Tfcs_e RCL_CmdBleCs_Tfcs |
| typedef enum RCL_CMD_BLE_CS_Tpm_e RCL_CmdBleCs_Tpm |
| typedef enum RCL_CMD_BLE_CS_Tip_e RCL_CmdBleCs_Tip |
| typedef enum RCL_CMD_BLE_CS_Tsw_e RCL_CmdBleCs_Tsw |
| typedef enum RCL_CMD_BLE_CS_AntennaConfig_e RCL_CmdBleCs_AntennaConfig |
| typedef enum RCL_CMD_BLE_CS_Payload_e RCL_CmdBleCs_Payload |
| typedef enum RCL_CMD_BLE_CS_RxGain_e RCL_CmdBleCs_RxGain |
| typedef enum RCL_CMD_BLE_CS_ToneQuality_e RCL_CmdBleCs_ToneQuality |
| typedef enum RCL_CMD_BLE_CS_ReportFormat_e RCL_CmdBleCs_ReportFormat |
| typedef enum RCL_CMD_BLE_CS_PacketAntenna_e RCL_CmdBleCs_PacketAntenna |
| typedef enum RCL_CMD_BLE_CS_Nadm_e RCL_CmdBleCs_Nadm |
| typedef void(* RCL_CmdBleCs_PrecalCallback) (RCL_CmdBleCs_PrecalTable *table, uint8_t channel, RCL_CmdBleCs_IQSample *pHigh, RCL_CmdBleCs_IQSample *pLow) |
Callback function for DC precalibration feature.
Describes the method that can select the right compensation value from the available precalibration table.
| enum RCL_CMD_BLE_CS_Phy_e |
Enumerator of packet status options.
Describes the available packet status words
| enum RCL_CMD_BLE_CS_Tpm_e |
| enum RCL_CMD_BLE_CS_Tip_e |
| enum RCL_CMD_BLE_CS_Tsw_e |
Enumerator of antenna configuration.
Describes the available values for configuration of antenna control for PCT measurement.
| void RCL_Handler_BLE_CS_PrecalDefaultCallback | ( | RCL_CmdBleCs_PrecalTable * | table, |
| uint8_t | channel, | ||
| RCL_CmdBleCs_IQSample * | pHigh, | ||
| RCL_CmdBleCs_IQSample * | pLow | ||
| ) |
References BLE_CS_MAX_CHANNEL.
| struct RCL_CMD_BLE_CS_SUBEVENT_RESULTS_t __attribute__ | ( | (packed) | ) |
| uint8_t subeventCode |
| uint16_t connectionHandle |
| uint8_t configID |
| uint16_t startAclConnectionEvent |
| uint16_t procedureCounter |
| int16_t frequencyCompensation |
| int8_t referencePowerLevel |
| uint8_t procedureDoneStatus |
| uint8_t subeventDoneStatus |
| uint8_t abortReason |
| uint8_t numAntennaPath |
| uint8_t numStepsReported |
| uint8_t data |
Referenced by RCL_Handler_BLE_CS_Precal(), RCL_IEEE_readPartialFrame(), RCL_MultiBuffer_init(), and RCL_TxBuffer_init().
| void __attribute__ |
| uint8_t mode |
Referenced by RCL_Handler_BLE_CS_convertRtt(), and RCL_Handler_BLE_CS_convertStepResult().
| uint8_t channel |
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_aux_adv(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_findAdvChannel(), RCL_Handler_BLE5_findRfFreq(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_periodicAdv(), RCL_Handler_BLE5_periodicScan(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), and RCL_Handler_BLE_CS_convertStepResult().
| uint8_t dataLength |
Referenced by RCL_Handler_BLE_CS_convertStepResult(), and RCL_Handler_BLE_CS_readS2RSamples().