|
| #define | ZB_ZCL_GENERAL_GET_NEXT_READ_ATTR_RES(data_buf, read_attr_resp) |
| | Parses Read attribute response and returns next Read attribute status record or NULL if there is no more data. More...
|
| |
| #define | ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ(buffer, cmd_ptr, def_resp) |
| | Initialize Read attribute command. More...
|
| |
| #define | ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_A(buffer, cmd_ptr, direction, def_resp) |
| | Initialize Read Attribute Request command. More...
|
| |
| #define | ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_MANUF(buffer, cmd_ptr, direction, def_resp, manuf_code) |
| | Initialize Read Attribute Request command with manufacturer code. More...
|
| |
| #define | ZB_ZCL_GENERAL_ADD_ID_READ_ATTR_REQ(cmd_ptr, attr_id) |
| | Add attribute id to command payload. More...
|
| |
| #define | ZB_ZCL_GENERAL_SEND_READ_ATTR_REQ(buffer, cmd_ptr, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb) |
| | Sends Read attribute command. More...
|
| |
| #define | ZB_ZCL_GENERAL_GET_READ_ATTR_REQ(_data_buf, _read_attr_req) |
| | Parses Read attribute request and returns next Read attribute record or NULL if there is no more data. More...
|
| |
| #define | ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP(_buffer, _cmd_ptr, _seq) |
| | Initialize Read Attribute Response command. More...
|
| |
| #define | ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP_EXT(_buffer, _cmd_ptr, _direction, _seq, _is_manuf, _manuf_id) |
| | Initialize Read Attribute Response command. More...
|
| |
| #define | ZB_ZCL_GENERAL_SEND_READ_ATTR_RESP( _buffer, _cmd_ptr, _addr, _dst_addr_mode, _dst_ep, _ep, _profile_id, _cluster_id, _cb) |
| | Send Read attribute response command. More...
|
| |
Read attributes command described in ZCL spec, subclauses 2.4.1 and 2.4.2.
Read attributes request command can be formed and sent as in following snippet:
Read attributes response can be parsed as:
until allocated buffer space exceeds.
Read attributes request parsing and response filling and sending is implemented in ZCL library internal functions.
§ ZB_ZCL_GENERAL_ADD_ID_READ_ATTR_REQ
| #define ZB_ZCL_GENERAL_ADD_ID_READ_ATTR_REQ |
( |
|
cmd_ptr, |
|
|
|
attr_id |
|
) |
| |
§ ZB_ZCL_GENERAL_GET_NEXT_READ_ATTR_RES
| #define ZB_ZCL_GENERAL_GET_NEXT_READ_ATTR_RES |
( |
|
data_buf, |
|
|
|
read_attr_resp |
|
) |
| |
§ ZB_ZCL_GENERAL_GET_READ_ATTR_REQ
| #define ZB_ZCL_GENERAL_GET_READ_ATTR_REQ |
( |
|
_data_buf, |
|
|
|
_read_attr_req |
|
) |
| |
#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>
Value:{ \
\
if ((_read_attr_req)) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(_read_attr_req)->attr_id); \
} \
}
struct zb_zcl_read_attr_req_s zb_zcl_read_attr_req_t
ZCL Read Attribute Command frame.
#define zb_buf_cut_left(buf, size)
Definition: zboss_api_buf.h:474
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
ZCL Read Attribute Command frame.
Definition: zb_zcl_commands.h:594
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372
Parses Read attribute request and returns next Read attribute record or NULL if there is no more data.
If request contains invalid data, NULL is returned.
- Parameters
-
| _data_buf | - ID zb_bufid_t of a buffer containing write attribute request data |
| _read_attr_req | - out pointer to zb_zcl_read_attr_req_t, containing Read attribute record out value direct into data_buf. Do not change data_buf before finish work with read_attr_req |
- Note
- data_buf buffer should contain Read attribute request payload, without ZCL header. Each parsed Read attribute record is extracted from initial data_buf buffer
§ ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ
| #define ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ |
( |
|
buffer, |
|
|
|
cmd_ptr, |
|
|
|
def_resp |
|
) |
| |
§ ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_A
| #define ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_A |
( |
|
buffer, |
|
|
|
cmd_ptr, |
|
|
|
direction, |
|
|
|
def_resp |
|
) |
| |
§ ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_MANUF
| #define ZB_ZCL_GENERAL_INIT_READ_ATTR_REQ_MANUF |
( |
|
buffer, |
|
|
|
cmd_ptr, |
|
|
|
direction, |
|
|
|
def_resp, |
|
|
|
manuf_code |
|
) |
| |
#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>
Value:{ \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1468
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1548
#define ZB_ZCL_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1018
#define ZB_ZCL_CMD_READ_ATTRIB
Definition: zb_zcl_commands.h:61
#define ZB_TRUE
Definition: zb_types.h:350
Initialize Read Attribute Request command with manufacturer code.
- Parameters
-
| buffer | - buffer to store command data |
| cmd_ptr | - pointer to a command data memory |
| direction | - direction of command (see zcl_frame_direction) |
| def_resp | - enable/disable default response |
| manuf_code | - manufacturer specific code |
§ ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP
| #define ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP |
( |
|
_buffer, |
|
|
|
_cmd_ptr, |
|
|
|
_seq |
|
) |
| |
§ ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP_EXT
| #define ZB_ZCL_GENERAL_INIT_READ_ATTR_RESP_EXT |
( |
|
_buffer, |
|
|
|
_cmd_ptr, |
|
|
|
_direction, |
|
|
|
_seq, |
|
|
|
_is_manuf, |
|
|
|
_manuf_id |
|
) |
| |
§ ZB_ZCL_GENERAL_SEND_READ_ATTR_REQ
| #define ZB_ZCL_GENERAL_SEND_READ_ATTR_REQ |
( |
|
buffer, |
|
|
|
cmd_ptr, |
|
|
|
addr, |
|
|
|
dst_addr_mode, |
|
|
|
dst_ep, |
|
|
|
ep, |
|
|
|
profile_id, |
|
|
|
cluster_id, |
|
|
|
cb |
|
) |
| |
§ ZB_ZCL_GENERAL_SEND_READ_ATTR_RESP
| #define ZB_ZCL_GENERAL_SEND_READ_ATTR_RESP |
( |
|
_buffer, |
|
|
|
_cmd_ptr, |
|
|
|
_addr, |
|
|
|
_dst_addr_mode, |
|
|
|
_dst_ep, |
|
|
|
_ep, |
|
|
|
_profile_id, |
|
|
|
_cluster_id, |
|
|
|
_cb |
|
) |
| |
§ zb_zcl_read_attr_req_t
§ zb_zcl_read_attr_res_t