Logo
Developing with ZBOSS for Zigbee
Prepayment cluster commands

Data Structures

struct  zb_zcl_prepayment_select_available_emergency_credit_payload_s
 
struct  zb_zcl_prepayment_change_debt_command_payload_s
 
struct  zb_zcl_prepayment_emergency_credit_setup_payload_s
 
struct  zb_zcl_prepayment_consumer_top_up_payload_s
 
struct  zb_zcl_prepayment_credit_adjustment_payload_s
 
struct  zb_zcl_prepayment_change_payment_mode_payload_s
 
struct  zb_zcl_prepayment_get_prepay_snapshot_payload_s
 
struct  zb_zcl_prepayment_get_top_up_log_payload_s
 
struct  zb_zcl_prepayment_get_debt_repayment_log_payload_s
 
struct  zb_zcl_prepayment_set_maximum_credit_limit_payload_s
 
struct  zb_zcl_prepayment_set_overall_debt_cap_payload_s
 
struct  zb_zcl_prepayment_snapshot_payload_s
 
struct  zb_zcl_prepayment_publish_prepay_snapshot_payload_s
 
struct  zb_zcl_prepayment_payment_mode_response_payload_s
 
struct  zb_zcl_prepayment_consumer_top_up_response_payload_s
 
struct  zb_zcl_prepayment_top_up_payload_details_s
 
struct  zb_zcl_prepayment_publish_top_up_log_payload_s
 
struct  zb_zcl_prepayment_debt_payload_record_s
 
struct  zb_zcl_prepayment_publish_debt_log_payload_s
 

Typedefs

typedef enum zb_zcl_prepayment_cli_cmd_e zb_zcl_prepayment_cli_cmd_t
 
typedef enum zb_zcl_prepayment_originating_device_e zb_zcl_prepayment_originating_device_t
 
typedef struct zb_zcl_prepayment_select_available_emergency_credit_payload_s zb_zcl_prepayment_select_available_emergency_credit_payload_t
 
typedef enum zb_zcl_prepayment_debt_amount_type_e zb_zcl_prepayment_debt_amount_type_t
 
typedef struct zb_zcl_prepayment_change_debt_command_payload_s zb_zcl_prepayment_change_debt_command_payload_t
 
typedef struct zb_zcl_prepayment_emergency_credit_setup_payload_s zb_zcl_prepayment_emergency_credit_setup_payload_t
 
typedef struct zb_zcl_prepayment_consumer_top_up_payload_s zb_zcl_prepayment_consumer_top_up_payload_t
 
typedef enum zb_zcl_prepayment_credit_type_e zb_zcl_prepayment_credit_type_t
 
typedef struct zb_zcl_prepayment_credit_adjustment_payload_s zb_zcl_prepayment_credit_adjustment_payload_t
 
typedef struct zb_zcl_prepayment_change_payment_mode_payload_s zb_zcl_prepayment_change_payment_mode_payload_t
 
typedef struct zb_zcl_prepayment_get_prepay_snapshot_payload_s zb_zcl_prepayment_get_prepay_snapshot_payload_t
 
typedef struct zb_zcl_prepayment_get_top_up_log_payload_s zb_zcl_prepayment_get_top_up_log_payload_t
 
typedef zb_uint32_t zb_zcl_prepayment_set_low_credit_warning_level_payload_t
 
typedef enum zb_zcl_prepayment_debt_type_e zb_zcl_prepayment_debt_type_t
 
typedef struct zb_zcl_prepayment_get_debt_repayment_log_payload_s zb_zcl_prepayment_get_debt_repayment_log_payload_t
 
typedef struct zb_zcl_prepayment_set_maximum_credit_limit_payload_s zb_zcl_prepayment_set_maximum_credit_limit_payload_t
 
typedef struct zb_zcl_prepayment_set_overall_debt_cap_payload_s zb_zcl_prepayment_set_overall_debt_cap_payload_t
 
typedef enum zb_zcl_prepayment_srv_cmd_e zb_zcl_prepayment_srv_cmd_t
 
typedef enum zb_zcl_prepayment_snapshot_payload_cause_e zb_zcl_prepayment_snapshot_payload_cause_t
 
typedef enum zb_zcl_prepayment_snapshot_payload_type_e zb_zcl_prepayment_snapshot_payload_type_t
 
typedef struct zb_zcl_prepayment_snapshot_payload_s zb_zcl_prepayment_snapshot_payload_t
 
typedef struct zb_zcl_prepayment_publish_prepay_snapshot_payload_s zb_zcl_prepayment_publish_prepay_snapshot_payload_t
 
typedef enum zb_zcl_prepayment_friendly_credit_bitmap_e zb_zcl_prepayment_friendly_credit_bitmap_t
 
typedef struct zb_zcl_prepayment_payment_mode_response_payload_s zb_zcl_prepayment_payment_mode_response_payload_t
 
typedef enum zb_zcl_prepayment_result_type_e zb_zcl_prepayment_result_type_t
 
typedef struct zb_zcl_prepayment_consumer_top_up_response_payload_s zb_zcl_prepayment_consumer_top_up_response_payload_t
 
typedef struct zb_zcl_prepayment_top_up_payload_details_s zb_zcl_prepayment_top_up_payload_details_t
 
typedef struct zb_zcl_prepayment_publish_top_up_log_payload_s zb_zcl_prepayment_publish_top_up_log_payload_t
 
typedef struct zb_zcl_prepayment_debt_payload_record_s zb_zcl_prepayment_debt_payload_record_t
 
typedef struct zb_zcl_prepayment_publish_debt_log_payload_s zb_zcl_prepayment_publish_debt_log_payload_t
 

Enumerations

enum  zb_zcl_prepayment_cli_cmd_e {
  ZB_ZCL_PREPAYMENT_CLI_CMD_SELECT_AVAILABLE_EMERGENCY_CREDIT = 0x00, ZB_ZCL_PREPAYMENT_CLI_CMD_CHANGE_DEBT = 0x02, ZB_ZCL_PREPAYMENT_CLI_CMD_EMERGENCY_CREDIT_SETUP, ZB_ZCL_PREPAYMENT_CLI_CMD_CONSUMER_TOP_UP,
  ZB_ZCL_PREPAYMENT_CLI_CMD_CREDIT_ADJUSTMENT, ZB_ZCL_PREPAYMENT_CLI_CMD_CHANGE_PAYMENT_MODE, ZB_ZCL_PREPAYMENT_CLI_CMD_GET_PREPAY_SNAPSHOT, ZB_ZCL_PREPAYMENT_CLI_CMD_GET_TOP_UP_LOG,
  ZB_ZCL_PREPAYMENT_CLI_CMD_SET_LOW_CREDIT_WARNING_LEVEL, ZB_ZCL_PREPAYMENT_CLI_CMD_GET_DEBT_REPAYMENT_LOG, ZB_ZCL_PREPAYMENT_CLI_CMD_SET_MAXIMUM_CREDIT_LIMIT, ZB_ZCL_PREPAYMENT_CLI_CMD_SET_OVERALL_DEBT_CAP
}
 
enum  zb_zcl_prepayment_originating_device_e { ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_ESI = 0x00, ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_METERING, ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_IHD }
 
enum  zb_zcl_prepayment_debt_amount_type_e {
  ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_1_ABSOLUTE = 0x00, ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_1_INCREMENTAL, ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_2_ABSOLUTE, ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_2_INCREMENTAL,
  ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_3_ABSOLUTE, ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_3_INCREMENTAL
}
 
enum  zb_zcl_prepayment_credit_type_e { ZB_ZCL_PREPAYMENT_CREDIT_INCREMENTAL = 0x00, ZB_ZCL_PREPAYMENT_CREDIT_ABSOLUTE }
 
enum  zb_zcl_prepayment_debt_type_e { ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_1 = 0x00, ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_2, ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_3, ZB_ZCL_PREPAYMENT_DEBT_TYPE_ALL_DEBTS = 0xFF }
 
enum  zb_zcl_prepayment_srv_cmd_e {
  ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_PREPAY_SNAPSHOT = 0x01, ZB_ZCL_PREPAYMENT_SRV_CMD_CHANGE_PAYMENT_MODE_RESPONSE, ZB_ZCL_PREPAYMENT_SRV_CMD_CONSUMER_TOP_UP_RESPONSE, ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_TOP_UP_LOG = 0x05,
  ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_DEBT_LOG
}
 
enum  zb_zcl_prepayment_snapshot_payload_cause_e {
  ZB_ZCL_PREPAYMENT_CAUSE_GENERAL = 1 << 0, ZB_ZCL_PREPAYMENT_CAUSE_END_OF_BILLING_PERIOD = 1 << 1, ZB_ZCL_PREPAYMENT_CAUSE_TARIFF_INFORMATION_CHANGE = 1 << 3, ZB_ZCL_PREPAYMENT_CAUSE_PRICE_MATRIX_CHANGE = 1 << 4,
  ZB_ZCL_PREPAYMENT_CAUSE_MANUALLY_TRIGGERED_FROM_CLIENT = 1 << 10, ZB_ZCL_PREPAYMENT_CAUSE_TENANCY_CHANGE = 1 << 12, ZB_ZCL_PREPAYMENT_CAUSE_SUPPLIER_CHANGE = 1 << 13, ZB_ZCL_PREPAYMENT_CAUSE_METER_MODE_CHANGE = 1 << 14,
  ZB_ZCL_PREPAYMENT_CAUSE_TOP_UP_ADDITION = 1 << 18, ZB_ZCL_PREPAYMENT_CAUSE_DEBT_AND_CREDIT_ADDITION = 1 << 19
}
 
enum  zb_zcl_prepayment_snapshot_payload_type_e { ZB_ZCL_PREPAYMENT_SNAPSHOT_PAYLOAD_TYPE_DEBT_AND_CREDIT_STATUS = 0x00 }
 
enum  zb_zcl_prepayment_friendly_credit_bitmap_e { PREPAYMENT_FRIENDLY_CREDIT_ENABLED = 0 }
 
enum  zb_zcl_prepayment_result_type_e {
  ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED = 0x00, ZB_ZCL_PREPAYMENT_RESULT_REJECTED_INVALID_TOP_UP, ZB_ZCL_PREPAYMENT_RESULT_REJECTED_DUPLICATE_TOP_UP, ZB_ZCL_PREPAYMENT_RESULT_REJECTED_ERROR,
  ZB_ZCL_PREPAYMENT_RESULT_REJECTED_MAX_CREDIT_REACHED, ZB_ZCL_PREPAYMENT_RESULT_REJECTED_KAYPAD_LOCK, ZB_ZCL_PREPAYMENT_RESULT_REJECTED_TOP_UP_VALUE_TOO_LARGE, ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_ENABLED = 0x10,
  ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_DISABLED, ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_ARMED
}
 

Detailed Description

Typedef Documentation

§ zb_zcl_prepayment_change_debt_command_payload_t

§ zb_zcl_prepayment_change_payment_mode_payload_t

§ zb_zcl_prepayment_cli_cmd_t

§ zb_zcl_prepayment_consumer_top_up_payload_t

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Consumer Top Up Command is used by the IHD and the ESI as a method to apply credit top up values to a prepayment meter.

See also
SE spec, subclause D.7.2.3.5

§ zb_zcl_prepayment_consumer_top_up_response_payload_t

§ zb_zcl_prepayment_credit_adjustment_payload_t

§ zb_zcl_prepayment_credit_type_t

§ zb_zcl_prepayment_debt_amount_type_t

§ zb_zcl_prepayment_debt_payload_record_t

§ zb_zcl_prepayment_debt_type_t

§ zb_zcl_prepayment_emergency_credit_setup_payload_t

§ zb_zcl_prepayment_friendly_credit_bitmap_t

§ zb_zcl_prepayment_get_debt_repayment_log_payload_t

§ zb_zcl_prepayment_get_prepay_snapshot_payload_t

§ zb_zcl_prepayment_get_top_up_log_payload_t

§ zb_zcl_prepayment_originating_device_t

§ zb_zcl_prepayment_payment_mode_response_payload_t

§ zb_zcl_prepayment_publish_debt_log_payload_t

§ zb_zcl_prepayment_publish_prepay_snapshot_payload_t

§ zb_zcl_prepayment_publish_top_up_log_payload_t

§ zb_zcl_prepayment_result_type_t

§ zb_zcl_prepayment_select_available_emergency_credit_payload_t

§ zb_zcl_prepayment_set_low_credit_warning_level_payload_t

§ zb_zcl_prepayment_set_maximum_credit_limit_payload_t

§ zb_zcl_prepayment_set_overall_debt_cap_payload_t

§ zb_zcl_prepayment_snapshot_payload_cause_t

§ zb_zcl_prepayment_snapshot_payload_t

§ zb_zcl_prepayment_snapshot_payload_type_t

§ zb_zcl_prepayment_srv_cmd_t

§ zb_zcl_prepayment_top_up_payload_details_t

Enumeration Type Documentation

§ zb_zcl_prepayment_cli_cmd_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Commands are generated by Prepayment Client.

See also
SE spec, subclause 7.2.3
Enumerator
ZB_ZCL_PREPAYMENT_CLI_CMD_SELECT_AVAILABLE_EMERGENCY_CREDIT 

This command is sent to the Metering Device to activate the use of any Emergency Credit available on the Metering Device.

ZB_ZCL_PREPAYMENT_CLI_CMD_CHANGE_DEBT 

The ChangeDebt command is sent to the Metering Device to change the debt values.

ZB_ZCL_PREPAYMENT_CLI_CMD_EMERGENCY_CREDIT_SETUP 

This command provides a method to set up the parameters for the Emergency Credit.

ZB_ZCL_PREPAYMENT_CLI_CMD_CONSUMER_TOP_UP 

The follow command is used by the IHD and the ESI as a method to apply credit top up values to a prepayment meter.

ZB_ZCL_PREPAYMENT_CLI_CMD_CREDIT_ADJUSTMENT 

The follow command is sent to update the Credit Remaining attribute on a Prepayment meter. It shall only be sent from an ESI to the Meter.

ZB_ZCL_PREPAYMENT_CLI_CMD_CHANGE_PAYMENT_MODE 

This command is sent to a Metering Device to instruct it to change its mode of operation, e.g. from Credit to Prepayment.

ZB_ZCL_PREPAYMENT_CLI_CMD_GET_PREPAY_SNAPSHOT 

This command is used to request the cluster server for snapshot data.

ZB_ZCL_PREPAYMENT_CLI_CMD_GET_TOP_UP_LOG 

This command is sent to the Metering Device to retrieve the log of Top Up codes received by the meter.

ZB_ZCL_PREPAYMENT_CLI_CMD_SET_LOW_CREDIT_WARNING_LEVEL 

This command is sent from client to a Prepayment server to set the warning level for low credit.

ZB_ZCL_PREPAYMENT_CLI_CMD_GET_DEBT_REPAYMENT_LOG 

This command is used to request the contents of the Repayment log.

ZB_ZCL_PREPAYMENT_CLI_CMD_SET_MAXIMUM_CREDIT_LIMIT 

This command is sent from a client to the Prepayment server to set the maximum credit level allowed in the meter.

ZB_ZCL_PREPAYMENT_CLI_CMD_SET_OVERALL_DEBT_CAP 

This command is sent from a client to the Prepayment server to set the overall debt cap allowed in the meter.

§ zb_zcl_prepayment_credit_type_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Credit Type Field Enumerations

See also
SE spec, Table D-148
Enumerator
ZB_ZCL_PREPAYMENT_CREDIT_INCREMENTAL 
ZB_ZCL_PREPAYMENT_CREDIT_ABSOLUTE 

§ zb_zcl_prepayment_debt_amount_type_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Debt Amount Type Field Enumerations

See also
SE spec, Table D-147
Enumerator
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_1_ABSOLUTE 
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_1_INCREMENTAL 
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_2_ABSOLUTE 
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_2_INCREMENTAL 
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_3_ABSOLUTE 
ZB_ZCL_PREPAYMENT_DEBT_AMOUNT_TYPE_3_INCREMENTAL 

§ zb_zcl_prepayment_debt_type_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Debt Type Field Enumerations

See also
SE spec, Table D-149
Enumerator
ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_1 
ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_2 
ZB_ZCL_PREPAYMENT_DEBT_TYPE_DEBT_3 
ZB_ZCL_PREPAYMENT_DEBT_TYPE_ALL_DEBTS 

§ zb_zcl_prepayment_friendly_credit_bitmap_e

§ zb_zcl_prepayment_originating_device_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Originating Device Field Enumerations

See also
SE spec, Table D-146
Enumerator
ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_ESI 
ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_METERING 
ZB_ZCL_PREPAYMENT_ORIGINATING_DEVICE_IHD 

§ zb_zcl_prepayment_result_type_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Result Type Field Enumerations

See also
SE spec, Table D-154
Enumerator
ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_INVALID_TOP_UP 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_DUPLICATE_TOP_UP 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_ERROR 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_MAX_CREDIT_REACHED 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_KAYPAD_LOCK 
ZB_ZCL_PREPAYMENT_RESULT_REJECTED_TOP_UP_VALUE_TOO_LARGE 
ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_ENABLED 
ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_DISABLED 
ZB_ZCL_PREPAYMENT_RESULT_ACCEPTED_SUPPLY_ARMED 

§ zb_zcl_prepayment_snapshot_payload_cause_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Snapshot Payload Cause

See also
SE spec, Table D-151
Enumerator
ZB_ZCL_PREPAYMENT_CAUSE_GENERAL 
ZB_ZCL_PREPAYMENT_CAUSE_END_OF_BILLING_PERIOD 
ZB_ZCL_PREPAYMENT_CAUSE_TARIFF_INFORMATION_CHANGE 
ZB_ZCL_PREPAYMENT_CAUSE_PRICE_MATRIX_CHANGE 
ZB_ZCL_PREPAYMENT_CAUSE_MANUALLY_TRIGGERED_FROM_CLIENT 
ZB_ZCL_PREPAYMENT_CAUSE_TENANCY_CHANGE 
ZB_ZCL_PREPAYMENT_CAUSE_SUPPLIER_CHANGE 
ZB_ZCL_PREPAYMENT_CAUSE_METER_MODE_CHANGE 
ZB_ZCL_PREPAYMENT_CAUSE_TOP_UP_ADDITION 
ZB_ZCL_PREPAYMENT_CAUSE_DEBT_AND_CREDIT_ADDITION 

§ zb_zcl_prepayment_snapshot_payload_type_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Snapshot Payload Type

See also
SE spec, Table D-152
Enumerator
ZB_ZCL_PREPAYMENT_SNAPSHOT_PAYLOAD_TYPE_DEBT_AND_CREDIT_STATUS 

§ zb_zcl_prepayment_srv_cmd_e

#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h>

Commands are generated by Prepayment Server.

See also
SE spec, subclause D.7.2.4
Enumerator
ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_PREPAY_SNAPSHOT 

This command is generated in response to a GetPrepaySnapshot command or when a new snapshot is created. It is used to return a single snapshot to the client.

ZB_ZCL_PREPAYMENT_SRV_CMD_CHANGE_PAYMENT_MODE_RESPONSE 

This command is sent in response to the ChangePaymentMode command. This command shall only inform the ESI of the current default setting that would affect the meter when entering into Prepayment/PAYG or Credit mode. Should these values require changing then other commands within the Prepayment & Price cluster should be used.

ZB_ZCL_PREPAYMENT_SRV_CMD_CONSUMER_TOP_UP_RESPONSE 
ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_TOP_UP_LOG 

This command is used to send the Top Up Code Log entries to the Prepayment client. The command shall be sent in response to a Get Top Up Log command and MAY be sent unsolicited whenever a new Top Up code is received and successfully processed

ZB_ZCL_PREPAYMENT_SRV_CMD_PUBLISH_DEBT_LOG 

This command is used to send the contents of the Repayment Log.