![]() |
![]() |
Structure for MCAN Rx FIFO Status. More...
#include <MCAN.h>
Data Fields | |
uint32_t | fillLvl |
uint32_t | getIdx |
uint32_t | putIdx |
uint32_t | fifoFull |
uint32_t | msgLost |
Structure for MCAN Rx FIFO Status.
uint32_t MCAN_RxFifoStatus::fillLvl |
Rx FIFO Fill Level - number of elements stored in Rx FIFO
uint32_t MCAN_RxFifoStatus::getIdx |
Rx FIFO Get Index
uint32_t MCAN_RxFifoStatus::putIdx |
Rx FIFO Put Index
uint32_t MCAN_RxFifoStatus::fifoFull |
Rx FIFO Full
0 = Rx FIFO not full
1 = Rx FIFO full
uint32_t MCAN_RxFifoStatus::msgLost |
Rx FIFO Message Lost