Data Fields
MCAN_HighPriorityMsgInfo Struct Reference

Structure for MCAN High Priority Message. More...

#include <MCAN.h>

Data Fields

uint32_t bufIdx
 
uint32_t msi
 
uint32_t filterIdx
 
uint32_t filterList
 

Detailed Description

Structure for MCAN High Priority Message.

Field Documentation

§ bufIdx

uint32_t MCAN_HighPriorityMsgInfo::bufIdx

Buffer Index. Only valid when MSI[1] = 1.

§ msi

uint32_t MCAN_HighPriorityMsgInfo::msi

Message Storage Indicator
0 = No FIFO selected
1 = FIFO message lost
2 = Message stored in FIFO 0
3 = Message stored in FIFO 1

§ filterIdx

uint32_t MCAN_HighPriorityMsgInfo::filterIdx

Filter Index

§ filterList

uint32_t MCAN_HighPriorityMsgInfo::filterList

Indicates the filter list of the matching filter element
0 = Standard Filter List
1 = Extended Filter List


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale