![]() |
![]() |
Structure for MCAN error logging counters status. More...
#include <MCAN.h>
Data Fields | |
uint32_t | transErrLogCnt |
uint32_t | recErrCnt |
uint32_t | rpStatus |
uint32_t | canErrLogCnt |
Structure for MCAN error logging counters status.
uint32_t MCAN_ErrCntStatus::transErrLogCnt |
Transmit Error Counter
uint32_t MCAN_ErrCntStatus::recErrCnt |
Receive Error Counter
uint32_t MCAN_ErrCntStatus::rpStatus |
Receive Error Passive
0 = The Receive Error Counter is below the error passive level (128)
1 = The Receive Error Counter has reached the error passive level (128)
uint32_t MCAN_ErrCntStatus::canErrLogCnt |
CAN Error Logging