![]() |
![]() |
I2CLPF3 Object. More...
#include <I2CLPF3.h>
Data Fields | |
I2C_BASE_OBJECT SwiP_Struct | swi |
uint32_t | bitRate |
uint8_t | sdaPin |
uint8_t | sclPin |
void * | i2cPostFxn |
Power_NotifyObj | i2cPostObj |
I2CLPF3 Object.
The application must not access any member variables of this structure!
I2C_BASE_OBJECT SwiP_Struct I2CLPF3_Object::swi |
uint32_t I2CLPF3_Object::bitRate |
uint8_t I2CLPF3_Object::sdaPin |
uint8_t I2CLPF3_Object::sclPin |
void* I2CLPF3_Object::i2cPostFxn |
Power_NotifyObj I2CLPF3_Object::i2cPostObj |