I2CLPF3 Pin Configuration. More...
#include <I2CLPF3.h>
Data Fields | |
uint8_t | pinSDA |
uint8_t | pinSCL |
I2CLPF3 Pin Configuration.
Pin configuration that holds non-default pins. The default pin configuration is typically defined in I2CLPF3_HWAttrs placed in the board file. The pin configuration structure is used by setting the custom void pointer in the I2C_Params to point to this struct. If the custom void pointer is NULL, the I2CLPF3_HWAttrs pin mapping will be used.
uint8_t I2CLPF3_I2CPinCfg::pinSDA |
uint8_t I2CLPF3_I2CPinCfg::pinSCL |