Struct to hold metadata for a crypto driver's operation.
More...
#include <HSMLPF3.h>
Struct to hold metadata for a crypto driver's operation.
HSMLPF3_acquireLock() populates the HSMLPF3_Operation.driverHandle while the rest of the metadata is populated by HSMLPF3_submitToken(). The HWI accesses this stored information to respond to the calling driver.
§ commandToken
Eip130Token_Command_t HSMLPF3_Operation::commandToken |
§ resultToken
Eip130Token_Result_t HSMLPF3_Operation::resultToken |
§ returnBehavior
§ callbackFxn
§ driverHandle
uintptr_t HSMLPF3_Operation::driverHandle |
The documentation for this struct was generated from the following file: