![]() |
![]() |
ECDSALPF3HSM Object. More...
#include <ECDSALPF3HSM.h>
Data Fields | |
CryptoKey * | key |
bool | isOpen |
ECDSA_ReturnBehavior | returnBehavior |
int_fast16_t | returnStatus |
ECDSA_CurveType | curveType |
ECDSA_DomainID | domainId |
ECDSA_CurveLength | curveLength |
ECDSA_DigestLength | digestLength |
ECDSA_OperationType | operationType |
ECDSA_Operation * | operation |
ECDSA_CallbackFxn | callbackFxn |
int_fast16_t | hsmStatus |
uint32_t | keyAssetID |
uint32_t | paramAssetID |
const uint8_t * | curveParam |
uint32_t | curveParamSize |
uint8_t * | input |
uint8_t | signature [144] |
ECDSALPF3HSM Object.
The application must not access any member variables of this structure!
CryptoKey* ECDSALPF3HSM_Object::key |
bool ECDSALPF3HSM_Object::isOpen |
ECDSA_ReturnBehavior ECDSALPF3HSM_Object::returnBehavior |
int_fast16_t ECDSALPF3HSM_Object::returnStatus |
ECDSA_CurveType ECDSALPF3HSM_Object::curveType |
ECDSA_DomainID ECDSALPF3HSM_Object::domainId |
ECDSA_CurveLength ECDSALPF3HSM_Object::curveLength |
ECDSA_DigestLength ECDSALPF3HSM_Object::digestLength |
ECDSA_OperationType ECDSALPF3HSM_Object::operationType |
ECDSA_Operation* ECDSALPF3HSM_Object::operation |
ECDSA_CallbackFxn ECDSALPF3HSM_Object::callbackFxn |
int_fast16_t ECDSALPF3HSM_Object::hsmStatus |
uint32_t ECDSALPF3HSM_Object::keyAssetID |
uint32_t ECDSALPF3HSM_Object::paramAssetID |
const uint8_t* ECDSALPF3HSM_Object::curveParam |
uint32_t ECDSALPF3HSM_Object::curveParamSize |
uint8_t* ECDSALPF3HSM_Object::input |
uint8_t ECDSALPF3HSM_Object::signature[144] |