These macros are reservations for I2C.h
§ I2C_STATUS_QUEUED
#define I2C_STATUS_QUEUED (1) |
I2C transaction is queued but has not started.
§ I2C_STATUS_SUCCESS
#define I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API.
§ I2C_STATUS_ERROR
#define I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API.
§ I2C_STATUS_UNDEFINEDCMD
#define I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes.
§ I2C_STATUS_TIMEOUT
#define I2C_STATUS_TIMEOUT (-3) |
§ I2C_STATUS_CLOCK_TIMEOUT
#define I2C_STATUS_CLOCK_TIMEOUT (-4) |
I2C serial clock line timeout.
§ I2C_STATUS_ADDR_NACK
#define I2C_STATUS_ADDR_NACK (-5) |
I2C target address not acknowledged.
§ I2C_STATUS_DATA_NACK
#define I2C_STATUS_DATA_NACK (-6) |
I2C data byte not acknowledged.
§ I2C_STATUS_ARB_LOST
#define I2C_STATUS_ARB_LOST (-7) |
I2C multi-controller arbitration lost.
§ I2C_STATUS_INCOMPLETE
#define I2C_STATUS_INCOMPLETE (-8) |
I2C transaction is in progress or returned without completing.
§ I2C_STATUS_BUS_BUSY
#define I2C_STATUS_BUS_BUSY (-9) |
I2C bus already in use by another controller. The I2C transaction was therefore unable to start.
§ I2C_STATUS_CANCEL
#define I2C_STATUS_CANCEL (-10) |
§ I2C_STATUS_INVALID_TRANS
#define I2C_STATUS_INVALID_TRANS (-11) |