![]() |
![]() |
Data Structures | |
union | ECC_BrainpoolP384R1_Param |
Union to access ECC_BrainpoolP384R1 curve params in bytes or words. More... | |
Macros | |
#define | ECCParams_BrainpoolP384R1_LENGTH 48 |
Length of BrainpoolP384R1 curve parameters in bytes. More... | |
Variables | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_generatorX |
X coordinate of the generator point of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_generatorY |
Y coordinate of the generator point of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_prime |
Prime of the generator point of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_a |
'a' constant of the ECC_BrainpoolP384R1 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_b |
'b' constant of the ECC_BrainpoolP384R1 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_order |
Order of the generator point of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_k_mont |
'k' in Montgomery domain of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_a_mont |
'a' in Montgomery domain of the ECC_BrainpoolP384R1 curve. More... | |
const ECC_BrainpoolP384R1_Param | ECC_BrainpoolP384R1_b_mont |
'b' in Montgomery domain of the ECC_BrainpoolP384R1 curve. More... | |
#define ECCParams_BrainpoolP384R1_LENGTH 48 |
Length of BrainpoolP384R1 curve parameters in bytes.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_generatorX |
X coordinate of the generator point of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_generatorY |
Y coordinate of the generator point of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_prime |
Prime of the generator point of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_a |
'a' constant of the ECC_BrainpoolP384R1 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b).
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_b |
'b' constant of the ECC_BrainpoolP384R1 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b).
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_order |
Order of the generator point of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_k_mont |
'k' in Montgomery domain of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_a_mont |
'a' in Montgomery domain of the ECC_BrainpoolP384R1 curve.
const ECC_BrainpoolP384R1_Param ECC_BrainpoolP384R1_b_mont |
'b' in Montgomery domain of the ECC_BrainpoolP384R1 curve.