![]() |
![]() |
PRELIMINARY VCE driver interface
WARNING These APIs are PRELIMINARY, and subject to change in the next few months.
The VCE driver allows you to interact with the Vector Compute Engine (VCE), a linear algebra accellerator peripheral using 64-bit complex numbers. Complex numbers are represented by the float complex type from complex.h, where each number is made up of two 32-bit floats. The VCE works with complex numbers in either Cartesian or Polar formats. In the Cartesian representation, the lower 32 bits are the real part and the upper 32 bits are the imaginary part. In Polar format, the lower 32 bits are the absolute part and the upper 32 bits are the angle, represented as pi radians. As long as arguments to the VCE functions use the same format, the result will also be in that format. Mixing formats produces wrong results. The driver provides basic data types for vectors and matrices constructed from float complex, as well as many common linear algebra operations on these data types.
All the vector/matrix operations can accept input and output pointers that are inside or outside VCE RAM. If all pointers provided to an operation are inside VCE RAM, the VCE will operate in scratchpad mode . This means the driver will assume that, given the current pointers, the input is already in VCE memory and that input and result will not overlap eachother. Therefore, no data will be copied, and the function output will be placed inside VCE memory. This is the most efficient way to utilize the VCE and is ideal for algorithms with multiple operations that feed into each other, such as MUSIC (https://en.wikipedia.org/wiki/MUSIC_(algorithm)). When chaining together operations, make sure as many as possible use vectors and matrices that are already in VCE memory, to prevent unnecessary copying and overhead.
If any of the pointers are outside VCE memory, the driver will copy input data to the start of its memory, place the result immediately following, and then copy the output back to the provided pointer. This may overwrite data that was already in this location.
The primary purpose of this driver is executing the MUSIC algorithm for distance estimation in Bluetooth Channel Sounding. An implementation of MUSIC using the VCE can be found in the vce_music example.
This section will cover driver usage.
#include <stddef.h>#include <stdint.h>#include <stdbool.h>#include <complex.h>#include <ti/drivers/dpl/HwiP.h>#include <ti/drivers/dpl/SemaphoreP.h>#include <ti/devices/DeviceFamily.h>#include <DeviceFamily_constructPath(inc/hw_memmap.h)>
Go to the source code of this file.
Data Structures | |
| struct | VCELPF3_ComplexVector |
| VCELPF3 Vector Struct. More... | |
| struct | VCELPF3_ComplexMatrix |
| VCELPF3 Matrix Struct. More... | |
| struct | VCELPF3_ComplexTriangleMatrix |
| VCELPF3 Upper Triangle Matrix Struct. More... | |
| struct | VCELPF3_Config |
| VCELPF3 Global configuration. More... | |
| struct | VCELPF3_HWAttrs |
| VCELPF3 Hardware attributes. More... | |
Macros | |
| #define | VCELPF3_STATUS_SUCCESS 0 |
| Successful status code. More... | |
| #define | VCELPF3_STATUS_ERROR 1 |
| Generic error status code. More... | |
| #define | VCELPF3_STATUS_RESOURCE_UNAVAILABLE 2 |
| An error status code returned if the hardware or software resource is currently unavailable. More... | |
| #define | VCELPF3_RESULT_INPLACE 0 |
| VCE operation is in-place, overwriting the input. More... | |
| #define | VCELPF3_MEM_BASE VCERAM_DATA0_BASE |
| Start of VCE RAM. More... | |
| #define | VCELPF3_MEM_SIZE_MIRRORED VCERAM_DATA0_SIZE |
| Size of VCE RAM in mirrored mode. More... | |
Enumerations | |
| enum | VCELPF3_OperationMode { VCELPF3_OperationMode_MIRRORED } |
| Define the VCE memory operation modes, which are the ways the VCE expects data to be stored in its memory. More... | |
| enum | VCELPF3_SchedulingMode { VCELPF3_SchedulingMode_PIPELINED } |
| Define the VCE memory scheduling modes, which are the ways VCE memory operations are scheduled and pipelined. More... | |
Functions | |
| void | VCELPF3_init (void) |
| VCE init function. More... | |
| void | VCELPF3_startOperationSequence () |
| VCE function to prepare the start of an operation chain. More... | |
| void | VCELPF3_stopOperationSequence () |
| VCE function to finish an operation chain. More... | |
| int_fast16_t | VCELPF3_dotProduct (VCELPF3_ComplexVector *vecA, VCELPF3_ComplexVector *vecB, bool conjugate, float complex *result) |
| VCE function for calculating the dot product of two vectors, with the option to perform the complex conjugate on the second vector first. More... | |
| int_fast16_t | VCELPF3_vectorMult (VCELPF3_ComplexVector *vecA, VCELPF3_ComplexVector *vecB, bool conjugate, VCELPF3_ComplexVector *result) |
| VCE function for calculating the element-wise product of two vectors, with the option to perform the complex conjugate on the second vector first. More... | |
| int_fast16_t | VCELPF3_vectorSum (VCELPF3_ComplexVector *vecA, VCELPF3_ComplexVector *vecB, VCELPF3_ComplexVector *result) |
| VCE function for calculating the element-wise sum of two vectors. More... | |
| int_fast16_t | VCELPF3_cartesianToPolarVector (VCELPF3_ComplexVector *vec, VCELPF3_ComplexVector *result) |
| VCE function for converting a complex vector in cartesian format to polar format. More... | |
| int_fast16_t | VCELPF3_polarToCartesianVector (VCELPF3_ComplexVector *vec, float complex *temp, VCELPF3_ComplexVector *result) |
| VCE function for converting a complex vector in polar format to cartesian format. More... | |
| int_fast16_t | VCELPF3_sortVector (VCELPF3_ComplexVector *vec, VCELPF3_ComplexVector *result) |
| VCE function for sorting the real parts of a complex vector in descending order. This function ignores the complex parts of each element and makes no guarantees to their contents after the operation is complete. More... | |
| int_fast16_t | VCELPF3_covMatrixSpatialSmoothing (VCELPF3_ComplexVector *vec, uint16_t covMatrixSize, bool fbAveraging, VCELPF3_ComplexTriangleMatrix *result) |
| VCE function for covariance matrix computation using spatial smoothing and optionally forward-backward averaging. More... | |
| int_fast16_t | VCELPF3_computeFFT (VCELPF3_ComplexVector *vec, bool inverse, VCELPF3_ComplexVector *result) |
| VCE function for computing the Discrete Fourier transform (DFT) of a complex vector using the Fast Fourier Transform (FFT) algorithm. Optionally, the Inverse DFT can be computed. Combines two VCE operations; first configuring the VCE for a fourier transform, then actually computing it. More... | |
| int_fast16_t | VCELPF3_matrixMult (VCELPF3_ComplexMatrix *matA, VCELPF3_ComplexMatrix *matB, VCELPF3_ComplexMatrix *result) |
| VCE function for multiplying two matrices. The number of rows in the first matrix must be equal to the number of columns in the second matrix. More... | |
| int_fast16_t | VCELPF3_matrixSum (VCELPF3_ComplexMatrix *matA, VCELPF3_ComplexMatrix *matB, VCELPF3_ComplexMatrix *result) |
| VCE function for adding two matrices. The matrices must be of exact same sizes. More... | |
| int_fast16_t | VCELPF3_matrixScalarSum (VCELPF3_ComplexMatrix *mat, float complex *scalar, VCELPF3_ComplexMatrix *result) |
| VCE function for adding a scalar to a each of a matrix' elements. More... | |
| int_fast16_t | VCELPF3_matrixScalarMult (VCELPF3_ComplexMatrix *mat, float complex *scalar, VCELPF3_ComplexMatrix *result) |
| VCE function for multiplying each of a matrix' elements by a scalar. More... | |
| int_fast16_t | VCELPF3_matrixNorm (VCELPF3_ComplexMatrix *mat, float complex *result) |
| Compute the Frobenius norm of a matrix. More... | |
| int_fast16_t | VCELPF3_jacobiEVD (VCELPF3_ComplexTriangleMatrix *mat, uint16_t maxIter, float stopThreshold, VCELPF3_ComplexVector *result) |
| VCE function to compute the Jacobi Eigen-Decomposition (EVD) of a triangular Hermitian Matrix. This results in a triangular, diagonal matrix of eigenvalues sorted in descending order replacing the original matrix, and a full matrix, where the eigenvectors are the columns. The eigenvector matrix can be placed anywhere in VCE memory except for where the input matrix is placed. When not using scratchpad mode, the eigenvector matrix will be placed next to the eigenvector matrix. More... | |
| int_fast16_t | VCELPF3_gaussJordanElim (VCELPF3_ComplexMatrix *mat, float zeroThreshold, VCELPF3_ComplexMatrix *result) |
| Reduce the input matrix A[MxN] to reduced echelon form using Gauss-Jordan Elimination. More... | |
| int_fast16_t | VCELPF3_unitCircle (uint16_t numPoints, uint16_t constant, uint16_t phase, bool conjugate, VCELPF3_ComplexVector *result) |
| Generate points evenly distributed on a unit circle VCE generates a unit circle as follow: exp(-j*2*pi*(k*M+phase)/1024 * (-1)^(conjugate)) More... | |
| void | VCELPF3_prepareResult (uint16_t resultSize, uint16_t inputSize, complex float *resultBuffer) |
| Configure the VCE pointers for temporary (in VCE memory) and final results for a VCE operation. This function is intended to be used inside VCE operations, such as dot product. More... | |
| uint16_t | VCELPF3_prepareVectors (VCELPF3_ComplexVector *vecA, VCELPF3_ComplexVector *vecB) |
| Configure the VCE for vector operation inputs. If not in scratchpad mode, the vectors are loaded one after the other into the start of VCE memory. More... | |
| uint16_t | VCELPF3_prepareMatrices (VCELPF3_ComplexMatrix *matA, VCELPF3_ComplexMatrix *matB) |
| Configure the VCE for matrix operation inputs. If not in scratchpad mode, the matrices are loaded one after the other into the start of VCE memory. More... | |
| void * | VCELPF3_loadTriangular (VCELPF3_ComplexMatrix *mat, uint16_t offset) |
| Loads the upper triangular part of a full matrix into VCE memory. More... | |
| void * | VCELPF3_loadArgMirrored (uint16_t argSize, uint16_t offset, float complex *src) |
| Load operation arguments into VCE memory, assuming the VCE is in mirrored mode. This means memory is viewed as one block that can fit 1024 complex numbers. More... | |
| #define VCELPF3_RESULT_INPLACE 0 |
VCE operation is in-place, overwriting the input.
| #define VCELPF3_MEM_BASE VCERAM_DATA0_BASE |
Start of VCE RAM.
| #define VCELPF3_MEM_SIZE_MIRRORED VCERAM_DATA0_SIZE |
Size of VCE RAM in mirrored mode.
| void VCELPF3_init | ( | void | ) |
VCE init function.
This function initializes the VCE internal state. It sets power dependencies, loads the necessary firmware, configures the VCE and sets up interrupts and semaphores
| void VCELPF3_startOperationSequence | ( | ) |
VCE function to prepare the start of an operation chain.
This function disables standby and acquire exclusive access to the VCE. It should be called before any sequence of VCE operations, wrapping them together with VCELPF3_stopOperationSequence(). VCE operations should not be called outside of a pair of VCELPF3_startOperationSequence() and VCELPF3_stopOperationSequence() functions.
| void VCELPF3_stopOperationSequence | ( | ) |
VCE function to finish an operation chain.
This function enables standby and releases exclusive access to the VCE. It should be called after any sequence of VCE operations, wrapping them together with VCELPF3_startOperationSequence(). VCE operations should not be called outside of a pair of VCELPF3_startOperationSequence() and VCELPF3_stopOperationSequence() functions.
| void VCELPF3_prepareResult | ( | uint16_t | resultSize, |
| uint16_t | inputSize, | ||
| complex float * | resultBuffer | ||
| ) |
Configure the VCE pointers for temporary (in VCE memory) and final results for a VCE operation. This function is intended to be used inside VCE operations, such as dot product.
| [in] | resultSize | the size of an operation result |
| [in] | inputSize | the size of an operation input |
| [out] | resultBuffer | a pointer where the operation result will be placed in VCE memory. If not using scratchpad mode, usually when an external buffer is supplied, configure to place the result at the start of VCE memory, before copying it to the buffer. |
| VCELPF3_STATUS_SUCCESS | The call was successful. |
| uint16_t VCELPF3_prepareVectors | ( | VCELPF3_ComplexVector * | vecA, |
| VCELPF3_ComplexVector * | vecB | ||
| ) |
Configure the VCE for vector operation inputs. If not in scratchpad mode, the vectors are loaded one after the other into the start of VCE memory.
| [in] | vecA | an input vector |
| [in] | vecB | an input vector, potentially the same as vecA |
| uint16_t VCELPF3_prepareMatrices | ( | VCELPF3_ComplexMatrix * | matA, |
| VCELPF3_ComplexMatrix * | matB | ||
| ) |
Configure the VCE for matrix operation inputs. If not in scratchpad mode, the matrices are loaded one after the other into the start of VCE memory.
| [in] | matA | a pointer to an input matrix |
| [in] | matB | a pointer to an input matrix, potentially the same as matA |
| void* VCELPF3_loadTriangular | ( | VCELPF3_ComplexMatrix * | mat, |
| uint16_t | offset | ||
| ) |
Loads the upper triangular part of a full matrix into VCE memory.
| [in] | mat | a pointer to a source matrix |
| [in] | offset | offset into VCE memory to load to |
| void* VCELPF3_loadArgMirrored | ( | uint16_t | argSize, |
| uint16_t | offset, | ||
| float complex * | src | ||
| ) |
Load operation arguments into VCE memory, assuming the VCE is in mirrored mode. This means memory is viewed as one block that can fit 1024 complex numbers.
| [in] | argSize | how many complex numbers to load |
| [in] | offset | offset into VCE memory to load to |
| [in] | src | data source pointer |