![]() |
![]() |
UART driver implementation for a Low Power F3 device UART controller.
============================================================================
The UART header file should be included in an application as follows:
Refer to UART2.h for a complete description of APIs and examples of use.
#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(inc/hw_types.h)>
#include <DeviceFamily_constructPath(driverlib/udma.h)>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/UART2.h>
Go to the source code of this file.
Data Structures | |
struct | UART2LPF3_HWAttrs |
UART2LPF3 Hardware attributes. More... | |
struct | UART2LPF3_Object |
UART2LPF3 Object. More... | |
Macros | |
#define | UART2LPF3_FIFO_SIZE 8 |
Typedefs | |
typedef struct UART2LPF3_Object * | UART2LPF3_Handle |
Enumerations | |
enum | UART2LPF3_CodingScheme { UART2LPF3_CODING_UART = 0, UART2LPF3_CODING_SIR = 1, UART2LPF3_CODING_SIR_LP = 2 } |
UART TXD/RXD encoding/decoding scheme. More... | |
#define UART2LPF3_FIFO_SIZE 8 |
Size of the TX and RX FIFOs is 8 items
typedef struct UART2LPF3_Object * UART2LPF3_Handle |
UART TXD/RXD encoding/decoding scheme.
Encoding scheme for data transmitted/received on TXD/RXD pins. The data can either be encoded as standard UART, or as an IrDA-compliant Serial Infrared stream, where the width of each pulse is 3/16th of the bit period. A low-power SIR encoding is also available, where the pulse width can be configured.
Enumerator | |
---|---|
UART2LPF3_CODING_UART | TXD/RXD coded as UART |
UART2LPF3_CODING_SIR | TXD/RXD coded as Serial Infrared |
UART2LPF3_CODING_SIR_LP | TXD/RXD coded as Low-Power Serial Infrared |