TI BLE5-Stack API Documentation  3.03.01.00
Data Fields
gapBondParams_t Struct Reference

Contains part of the GAP Bond Manager Parameters values. More...

Data Fields

uint8_t authenPairingOnly
 
uint8_t autoSyncAL
 
uint8_t bondFailAction
 
uint8_t bonding
 
uint8_t eccDebugKeys
 
uint8_t eccReGenPolicy
 
uint8_t eraseBondWhileInConn
 
uint8_t ioCap
 
uint8_t KeyDistList
 
uint8_t KeySize
 
uint8_t mitm
 
uint8_t pairMode
 
uint8_t removeLRUBond
 
uint8_t sameIrkAction
 
uint8_t secureConnection
 

Detailed Description

Contains part of the GAP Bond Manager Parameters values.


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale