Radio Control Layer (RCL)
|
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
union | RCL_Events |
struct | RCL_Events_u.__unnamed__ |
Macros | |
#define | RCL_EventNone ((RCL_Events){ .value = (0 << 0)}) |
#define | RCL_EventCmdStarted ((RCL_Events){ .value = (1 << 0)}) |
#define | RCL_EventLastCmdDone ((RCL_Events){ .value = (1 << 1)}) |
#define | RCL_EventRxEntryAvail ((RCL_Events){ .value = (1 << 2)}) |
#define | RCL_EventRxBufferFinished ((RCL_Events){ .value = (1 << 3)}) |
#define | RCL_EventTxBufferFinished ((RCL_Events){ .value = (1 << 4)}) |
#define | RCL_EventSoftwareTriggered ((RCL_Events){ .value = (1 << 5)}) |
#define | RCL_EventTimerStart ((RCL_Events){ .value = (1 << 6)}) |
#define | RCL_EventDescheduleStop ((RCL_Events){ .value = (1 << 7)}) |
#define | RCL_EventGracefulStop ((RCL_Events){ .value = (1 << 8)}) |
#define | RCL_EventHardStop ((RCL_Events){ .value = (1 << 9)}) |
#define | RCL_EventStopDelayed ((RCL_Events){ .value = (1 << 10)}) |
#define | RCL_EventStopRejected ((RCL_Events){ .value = (1 << 11)}) |
#define | RCL_EventStartDelayed ((RCL_Events){ .value = (1 << 12)}) |
#define | RCL_EventStartRejected ((RCL_Events){ .value = (1 << 13)}) |
#define | RCL_EventSetup ((RCL_Events){ .value = (1 << 14)}) |
#define | RCL_EventPartialSetup ((RCL_Events){ .value = (1 << 15)}) |
#define | RCL_EventRxBufferUpdate ((RCL_Events){ .value = (1 << 16)}) |
#define | RCL_EventTxBufferUpdate ((RCL_Events){ .value = (1 << 17)}) |
#define | RCL_EventHandlerCmdUpdate ((RCL_Events){ .value = (1 << 18)}) |
#define | RCL_EventCmdStepDone ((RCL_Events){ .value = (1 << 19)}) |
#define | RCL_EventStopTimesUpdated ((RCL_Events){ .value = (1 << 20)}) |
union RCL_Events_u |
Data Fields | ||
---|---|---|
struct RCL_Events_u | __unnamed__ | |
uint32_t | value |
struct RCL_Events_u.__unnamed__ |
Data Fields | ||
---|---|---|
uint32_t | cmdStarted: 1 |
Command handler has accepted and started executing |
uint32_t | lastCmdDone: 1 |
The RCL is finished with the command |
uint32_t | rxEntryAvail: 1 |
An RX entry has been made available |
uint32_t | rxBufferFinished: 1 |
An RX multi-buffer is finished |
uint32_t | txBufferFinished: 1 |
A TX buffer is finished |
uint32_t | swTriggered: 1 |
Handler is triggered from software |
uint32_t | timerStart: 1 |
Timer-based start signalled |
uint32_t | descheduleStop: 1 |
Deschedule-type stop signalled |
uint32_t | gracefulStop: 1 |
Timer/api-based graceful-stop signalled |
uint32_t | hardStop: 1 |
Timer/api-based hard-stop signalled |
uint32_t | stopDelayed: 1 |
Command was not stopped |
uint32_t | stopRejected: 1 |
Command was not stopped |
uint32_t | startDelayed: 1 |
Command start is delayed, may still happen within allowDelay |
uint32_t | startRejected: 1 |
Command start is not possible within scheduling parameters |
uint32_t | setup: 1 |
Setup has been performed |
uint32_t | partialSetup: 1 |
Partial setup has been performed or is required by the running command |
uint32_t | rxBufferUpdate: 1 |
RX buffer has been updated |
uint32_t | txBufferUpdate: 1 |
TX buffer has been updated |
uint32_t | handlerCmdUpdate: 1 |
A property of a running command has been updated, to be detailed by handler |
uint32_t | cmdStepDone: 1 |
A step of the command has been done; details are command specific |
uint32_t | stopTimesUpdated: 1 |
A change was made to the stop times |
#define RCL_EventNone ((RCL_Events){ .value = (0 << 0)}) |
#define RCL_EventCmdStarted ((RCL_Events){ .value = (1 << 0)}) |
Command handler has accepted and started executing
#define RCL_EventLastCmdDone ((RCL_Events){ .value = (1 << 1)}) |
The RCL is finished with the command
Referenced by RCL_AdcNoise_get_samples_callback().
#define RCL_EventRxEntryAvail ((RCL_Events){ .value = (1 << 2)}) |
An RX entry has been made available
#define RCL_EventRxBufferFinished ((RCL_Events){ .value = (1 << 3)}) |
An RX multi-buffer is finished
#define RCL_EventTxBufferFinished ((RCL_Events){ .value = (1 << 4)}) |
A TX buffer is finished
#define RCL_EventSoftwareTriggered ((RCL_Events){ .value = (1 << 5)}) |
Handler is triggered from software
Referenced by RCL_Scheduler_postEvent().
#define RCL_EventTimerStart ((RCL_Events){ .value = (1 << 6)}) |
Timer-based start signalled
#define RCL_EventDescheduleStop ((RCL_Events){ .value = (1 << 7)}) |
Deschedule-type stop signalled
#define RCL_EventGracefulStop ((RCL_Events){ .value = (1 << 8)}) |
Timer-based graceful-stop signalled
Referenced by rclStop().
#define RCL_EventHardStop ((RCL_Events){ .value = (1 << 9)}) |
Timer-based hard-stop signalled
Referenced by rclStop().
#define RCL_EventStopDelayed ((RCL_Events){ .value = (1 << 10)}) |
Command was not stopped
#define RCL_EventStopRejected ((RCL_Events){ .value = (1 << 11)}) |
Command was not stopped
#define RCL_EventStartDelayed ((RCL_Events){ .value = (1 << 12)}) |
Command start is delayed, may still happen within allowDelay
#define RCL_EventStartRejected ((RCL_Events){ .value = (1 << 13)}) |
Command start is not possible within scheduling parameters
#define RCL_EventSetup ((RCL_Events){ .value = (1 << 14)}) |
Setup has been performed
Referenced by RCL_Lite_Command_start(), and rclSchedulerHwi().
#define RCL_EventPartialSetup ((RCL_Events){ .value = (1 << 15)}) |
Partial setup has been performed or is required by the running command
#define RCL_EventRxBufferUpdate ((RCL_Events){ .value = (1 << 16)}) |
RX buffer has been updated
Referenced by RCL_MultiBuffer_put().
#define RCL_EventTxBufferUpdate ((RCL_Events){ .value = (1 << 17)}) |
TX buffer has been updated
Referenced by RCL_TxBuffer_put().
#define RCL_EventHandlerCmdUpdate ((RCL_Events){ .value = (1 << 18)}) |
A property of a running command has been updated, to be detailed by handler
Referenced by RCL_BLE5_updateFilterList(), RCL_IEEE_Tx_stop(), RCL_IEEE_Tx_submit(), and rclCommandHwi().
#define RCL_EventCmdStepDone ((RCL_Events){ .value = (1 << 19)}) |
A step of the command has been done; details are command specific
#define RCL_EventStopTimesUpdated ((RCL_Events){ .value = (1 << 20)}) |
A change was made to the stop times
Referenced by rclSchedulerCancelStopTime(), and rclSchedulerSetNewStopTime().