VCELPF3 Matrix Struct. More...
#include <VCELPF3.h>
Data Fields | |
complex float * | data |
uint16_t | rows |
uint16_t | cols |
VCELPF3 Matrix Struct.
Struct representing a column-major Matrix data type. Column-mjaor means that for an NxN matrix, N columns of size N will be stored after each other in memory.
complex float* VCELPF3_ComplexMatrix::data |
Pointer to the matrix data.
uint16_t VCELPF3_ComplexMatrix::rows |
Number of rows in the matrix.
uint16_t VCELPF3_ComplexMatrix::cols |
Number of columns in the matrix.