#include <TaskP.h>
Data Fields | |
char * | name |
void * | arg |
int | priority |
size_t | stackSize |
void * | stack |
Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL. More... | |
char* TaskP_Params::name |
Task name. Default: NAME
void* TaskP_Params::arg |
Task function argument. Default: NULL
int TaskP_Params::priority |
Task priority. Higher values represent higher priorities. Default: 0
size_t TaskP_Params::stackSize |
Task stack size. Default: TaskP_DEFAULT_STACK_SIZE
void* TaskP_Params::stack |
Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL.