Data Fields
TCAN455X_Config Struct Reference

TCAN455X global configuration. More...

#include <TCAN455X.h>

Data Fields

uint32_t clkFreqMHz
 
uint32_t spiBitRate
 
void * taskStack
 
uint16_t taskStackSize
 
uint8_t taskPri
 
uint_least8_t spiIndex
 
uint_least8_t spiCSPin
 
uint_least8_t interruptPin
 

Detailed Description

TCAN455X global configuration.

Field Documentation

§ clkFreqMHz

uint32_t TCAN455X_Config::clkFreqMHz

TCAN455X input clock frequency in MHz

§ spiBitRate

uint32_t TCAN455X_Config::spiBitRate

SPI bit rate to communicate with TCAN455X

§ taskStack

void* TCAN455X_Config::taskStack

Pointer to TCAN455X interrupt handler task stack

§ taskStackSize

uint16_t TCAN455X_Config::taskStackSize

TCAN455X interrupt handler task stack size

§ taskPri

uint8_t TCAN455X_Config::taskPri

TCAN455X interrupt handler task priority

§ spiIndex

uint_least8_t TCAN455X_Config::spiIndex

SPI instance index from Board file

§ spiCSPin

uint_least8_t TCAN455X_Config::spiCSPin

SPI Chip Select pin

§ interruptPin

uint_least8_t TCAN455X_Config::interruptPin

TCAN455X interrupt pin


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale