![]() |
![]() |
Basic SwiP Parameters. More...
#include <SwiP.h>
Data Fields | |
uintptr_t | arg0 |
uintptr_t | arg1 |
uint32_t | priority |
uint32_t | trigger |
Basic SwiP Parameters.
Structure that contains the parameters passed into SwiP_create and SwiP_construct when creating or constructing a SwiP instance. The SwiP_Params_init function should be used to initialize the fields to default values before the application sets the fields manually. The SwiP default parameters are noted in SwiP_Params_init.
Each SwiP object has a "trigger" used either to determine whether to post the SwiP or as a value that can be evaluated within the SwiP's function.
The SwiP_andn and SwiP_dec functions post the SwiP if the trigger value transitions to 0. The SwiP_or and SwiP_inc functions also modify the trigger value. SwiP_or sets bits, and SwiP_andn clears bits.
uintptr_t SwiP_Params::arg0 |
Argument passed into the SwiP function.
uintptr_t SwiP_Params::arg1 |
Argument passed into the SwiP function.
uint32_t SwiP_Params::priority |
priority, 0 is min, 1, 2, ..., ~0 for max
uint32_t SwiP_Params::trigger |
Initial SwiP trigger value.