Data Fields
NVS_Params Struct Reference

NVS Parameters. More...

#include <NVS.h>

Data Fields

void * custom
 

Detailed Description

NVS Parameters.

NVS parameters are used with the NVS_open() call. Default values for these parameters are set using NVS_Params_init().

See also
NVS_Params_init()

Field Documentation

§ custom

void* NVS_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale