![]() |
![]() |
Data Structures | |
union | ECC_NISTP521_Param |
Union to access ECC_NISTP521 curve params in bytes or words. More... | |
Macros | |
#define | ECCParams_NISTP521_LENGTH 66 |
Length of NIST P521 curve parameters in bytes. More... | |
#define | ECC_NISTP521_PARAM_LENGTH_WITH_PADDED_BYTES (ECCParams_NISTP521_LENGTH + HSM_PADDED_PARAM_BYTES) |
Length in bytes of NISTP521 curve parameters including the padded 0s so that the HSM is provided curve parameters with length that is divisible by 4, per its requirements. More... | |
Variables | |
const ECC_NISTP521_Param | ECC_NISTP521_generatorX |
X coordinate of the generator point of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_generatorY |
Y coordinate of the generator point of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_prime |
Prime of the generator point of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_a |
'a' constant of the ECC_NISTP521 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More... | |
const ECC_NISTP521_Param | ECC_NISTP521_b |
'b' constant of the ECC_NISTP521 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More... | |
const ECC_NISTP521_Param | ECC_NISTP521_order |
Order of the generator point of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_k_mont |
'k' in Montgomery domain of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_a_mont |
'a' in Montgomery domain of the ECC_NISTP521 curve. More... | |
const ECC_NISTP521_Param | ECC_NISTP521_b_mont |
'b' in Montgomery domain of the ECC_NISTP521 curve. More... | |
#define ECCParams_NISTP521_LENGTH 66 |
Length of NIST P521 curve parameters in bytes.
#define ECC_NISTP521_PARAM_LENGTH_WITH_PADDED_BYTES (ECCParams_NISTP521_LENGTH + HSM_PADDED_PARAM_BYTES) |
Length in bytes of NISTP521 curve parameters including the padded 0s so that the HSM is provided curve parameters with length that is divisible by 4, per its requirements.
const ECC_NISTP521_Param ECC_NISTP521_generatorX |
X coordinate of the generator point of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_generatorY |
Y coordinate of the generator point of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_prime |
Prime of the generator point of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_a |
'a' constant of the ECC_NISTP521 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b).
const ECC_NISTP521_Param ECC_NISTP521_b |
'b' constant of the ECC_NISTP521 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b).
const ECC_NISTP521_Param ECC_NISTP521_order |
Order of the generator point of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_k_mont |
'k' in Montgomery domain of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_a_mont |
'a' in Montgomery domain of the ECC_NISTP521 curve.
const ECC_NISTP521_Param ECC_NISTP521_b_mont |
'b' in Montgomery domain of the ECC_NISTP521 curve.