![]() |
![]() |
Macros | |
#define | VCELPF3_STATUS_SUCCESS 0 |
Successful status code. More... | |
#define | VCELPF3_STATUS_ERROR 1 |
Generic error status code. More... | |
#define | VCELPF3_STATUS_RESOURCE_UNAVAILABLE 2 |
An error status code returned if the hardware or software resource is currently unavailable. More... | |
#define VCELPF3_STATUS_SUCCESS 0 |
Successful status code.
#define VCELPF3_STATUS_ERROR 1 |
Generic error status code.
#define VCELPF3_STATUS_RESOURCE_UNAVAILABLE 2 |
An error status code returned if the hardware or software resource is currently unavailable.