Macros
UART2_EVENT

Macros

#define UART2_EVENT_OVERRUN   (0x08)
 A receive overrun has occurred. More...
 
#define UART2_EVENT_BREAK   (0x04)
 A break has occurred. More...
 
#define UART2_EVENT_PARITY   (0x02)
 A parity error has occurred. More...
 
#define UART2_EVENT_FRAMING   (0x01)
 A framing error has occurred. More...
 
#define UART2_EVENT_TX_BEGIN   (0x10)
 The UART will start transmitting data. More...
 
#define UART2_EVENT_TX_FINISHED   (0x20)
 The UART stopped transmitting data. More...
 

Detailed Description

Macro Definition Documentation

§ UART2_EVENT_OVERRUN

#define UART2_EVENT_OVERRUN   (0x08)

A receive overrun has occurred.

§ UART2_EVENT_BREAK

#define UART2_EVENT_BREAK   (0x04)

A break has occurred.

§ UART2_EVENT_PARITY

#define UART2_EVENT_PARITY   (0x02)

A parity error has occurred.

§ UART2_EVENT_FRAMING

#define UART2_EVENT_FRAMING   (0x01)

A framing error has occurred.

§ UART2_EVENT_TX_BEGIN

#define UART2_EVENT_TX_BEGIN   (0x10)

The UART will start transmitting data.

This event can be useful in RS-485 half-duplex systems to toggle TX enable high.

§ UART2_EVENT_TX_FINISHED

#define UART2_EVENT_TX_FINISHED   (0x20)

The UART stopped transmitting data.

This event can be useful in RS-485 half-duplex systems to toggle TX enable low.

© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale