![]() |
![]() |
Macros | |
#define | CAN_FILTER_RANGE ((uint32_t)0U) |
#define | CAN_FILTER_DUAL_ID ((uint32_t)1U) |
#define | CAN_FILTER_WITH_MASK ((uint32_t)2U) |
#define | CAN_FILTER_DISABLE ((uint32_t)3U) |
Filter Type for use with CAN_MsgRamConfig
0 = Range filter from SFID1 to SFID2 (SFID2 >= SFID1)
1 = Dual ID filter for SFID1 or SFID2
2 = Classic filter: SFID1 = filter, SFID2 = mask
3 = Filter element disabled
#define CAN_FILTER_RANGE ((uint32_t)0U) |
#define CAN_FILTER_DUAL_ID ((uint32_t)1U) |
#define CAN_FILTER_WITH_MASK ((uint32_t)2U) |
#define CAN_FILTER_DISABLE ((uint32_t)3U) |