![]() |
![]() |
Button driver.
The Button driver simplifies interfacing push buttons. For example, push buttons on LaunchPads, BoosterPacks, or custom boards may easily be managed via the Button API. A given button instance may subscribe to one or several Button_Events. When a subscribed event occurs, the user will receive a callback with the handle of the button and the event(s) that occured.
Buttons use the GPIO.h interface for interfacing with hardware, so a GPIO_PinConfig array must exist and contain a config for the button pin. The user must statically allocate a Button_Config array called Button_config. Each physical button should map to an index in Button_config.
Each structure must be defined by the application. The following example is for a MSP432 in which two buttons are setup. The following declarations are placed in "ti_drivers_config.h" and "ti_drivers_config.c" respectively. How the GPIO configs are defined are detailed in the next example.
"ti_drivers_config.c"
The following example is for a MSP432. We are showing interfacing of two push buttons. Each need a GPIO pin. The following definitions are in "ti_drivers_config.h" and "ti_drivers_config.c" respectively. This example uses GPIO pins 1.1 and 1.4. The other GPIO configuration structures must exist, see GPIO.h.
"ti_drivers_config.h"
"ti_drivers_config.c"
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/GPIO.h>
#include <ti/drivers/dpl/ClockP.h>
Go to the source code of this file.
Data Structures | |
struct | Button_Config |
Button configuration. More... | |
struct | Button_HWAttrs |
Hardware specific settings for a button. More... | |
struct | Button_Object |
Internal to Button module. Members should not be accessed by the application. More... | |
struct | Button_Params |
Button Parameters. More... | |
Typedefs | |
typedef struct Button_Config | Button_Config |
Button configuration. More... | |
typedef struct Button_Config * | Button_Handle |
A handle that is returned from a Button_open() call. More... | |
typedef enum Button_Events | Button_Events |
Button event flags. More... | |
typedef uint8_t | Button_EventMask |
Event subscription and notification mask type. More... | |
typedef void(* | Button_Callback) (Button_Handle buttonHandle, Button_EventMask buttonEvents) |
A handler to receive button callbacks. More... | |
typedef enum Button_Pull | Button_Pull |
Button Pull settings. More... | |
typedef struct Button_HWAttrs | Button_HWAttrs |
Hardware specific settings for a button. More... | |
typedef struct Button_Object | Button_Object |
Internal to Button module. Members should not be accessed by the application. More... | |
typedef struct Button_Params | Button_Params |
Button Parameters. More... | |
Enumerations | |
enum | Button_Events { Button_EV_PRESSED = 0x01, Button_EV_LONGPRESSED = 0x02, Button_EV_RELEASED = 0x04, Button_EV_CLICKED = 0x08, Button_EV_LONGCLICKED = 0x10, Button_EV_DOUBLECLICKED = 0x20 } |
Button event flags. More... | |
enum | Button_Pull { Button_PULL_DOWN = 0, Button_PULL_UP = 1 } |
Button Pull settings. More... | |
Functions | |
void | Button_close (Button_Handle handle) |
Function to close a Button specified by the Button_Handle. More... | |
void | Button_init (void) |
Function to initialize Button driver. More... | |
Button_Handle | Button_open (uint_least8_t buttonIndex, Button_Params *params) |
Function to open a given Button. More... | |
void | Button_Params_init (Button_Params *params) |
Function to initialize a Button_Params struct to its defaults. More... | |
uint32_t | Button_getLastPressedDuration (Button_Handle handle) |
Function to return the lastPressedDuration (valid only for short press, long press) More... | |
void | Button_setCallback (Button_Handle handle, Button_Callback buttonCallback) |
Function to set callback function for the button instance. More... | |
void | Button_gpioCallbackFxn (uint_least8_t index) |
This is the GPIO interrupt callback function which is called on a button press or release. This is internally used by button module. More... | |
Variables | |
const uint_least8_t | Button_count |
typedef struct Button_Config Button_Config |
Button configuration.
Each Button_Config represents a single physical button. It contains pointers to the button's Button_HWAttrs and Button_Object. The user must statically allocate all of these structures.
typedef struct Button_Config* Button_Handle |
A handle that is returned from a Button_open() call.
User will use this handle to interact with a given button instance.
typedef enum Button_Events Button_Events |
Button event flags.
The event flags can be used by the user to subscribe to specific kinds of button actions and by the driver to signal which event caused a callback.
typedef uint8_t Button_EventMask |
Event subscription and notification mask type.
typedef void(* Button_Callback) (Button_Handle buttonHandle, Button_EventMask buttonEvents) |
A handler to receive button callbacks.
typedef enum Button_Pull Button_Pull |
Button Pull settings.
This enumeration defines whether the button is active low (PULL_UP) or active high (PULL_DOWN) and is used to control internal logic.
typedef struct Button_HWAttrs Button_HWAttrs |
Hardware specific settings for a button.
This structure should be defined and provided by the application.
typedef struct Button_Object Button_Object |
Internal to Button module. Members should not be accessed by the application.
typedef struct Button_Params Button_Params |
Button Parameters.
Button parameters are used with the Button_open() call. Default values for these parameters are set using Button_Params_init().
enum Button_Events |
Button event flags.
The event flags can be used by the user to subscribe to specific kinds of button actions and by the driver to signal which event caused a callback.
enum Button_Pull |
void Button_close | ( | Button_Handle | handle | ) |
Function to close a Button specified by the Button_Handle.
[in] | handle | A Button_Handle returned from Button_open() call |
void Button_init | ( | void | ) |
Function to initialize Button driver.
Button_Handle Button_open | ( | uint_least8_t | buttonIndex, |
Button_Params * | params | ||
) |
Function to open a given Button.
Function to open a button instance corresponding to a Button_Config in the Button_config array. The GPIO configurations must exist prior to calling this function. The Button_Params may be used to specify runtime parameters.
[in] | buttonIndex | Logical button number indexed into the Button_config table |
[in] | *params | A pointer to Button_Params structure. If NULL, it will use default values. |
void Button_Params_init | ( | Button_Params * | params | ) |
Function to initialize a Button_Params struct to its defaults.
[in] | params | A pointer to a Button_Params structure that will be initialized. |
parameter | value | description | unit |
---|---|---|---|
debounceDuration | 10 | debounce duration | ms |
longPressDuration | 2000 | long press duration | ms |
buttonEventMask | 0xFF | subscribed to all events | NA |
uint32_t Button_getLastPressedDuration | ( | Button_Handle | handle | ) |
Function to return the lastPressedDuration (valid only for short press, long press)
The API returns last pressed duration and it is valid only for shortpress, longpress. If this API is called after receiving an event click or long click then the API returns the press duration which is time delta between the press and release of the button.
[in] | handle | Pointer to the Button_Handle of the desired button. |
void Button_setCallback | ( | Button_Handle | handle, |
Button_Callback | buttonCallback | ||
) |
Function to set callback function for the button instance.
[in] | handle | A Button_Handle returned from Button_open() |
[in] | buttonCallback | button callback function |
void Button_gpioCallbackFxn | ( | uint_least8_t | index | ) |
This is the GPIO interrupt callback function which is called on a button press or release. This is internally used by button module.
This function is internally used by button module for receiving the GPIO interrupt callbacks. This is exposed to the application for wake up cases. In some of the MCUs, when in LPDS(Low power deep sleep) the GPIO interrupt is consumed for wake up, and in order to make the button module work the the application has to call this API with the index of the GPIO pin which actually was the reason for the wake up.
[in] | index | Index of the GPIO for which the button press has to be detected. This is an index in GPIO_PinConfig array. |
const uint_least8_t Button_count |