Functions
Board.h File Reference

Detailed Description

Portable board-specific symbols.


The Board header file should be included in an application as follows:

This header serves as device-independent interface for applications using peripherals connected to the device via standard digital interfaces; e.g, GPIO, SPI, I2C, UART, etc. Its purpose is to enable application code that references a peripheral to be portable to any device and board that supports the peripheral.

Usage

Synopsis

void main(void)
{
:
}

Initializing the hardware

Board_init() must be called before any other driver API. This function is owned by the user (typically generated by SysConfig), and is responsible for device specific initialization; e.g., initializing clocks and power management functionality.

Go to the source code of this file.

Functions

void Board_init (void)
 Performs "early" board-level initialization required by TI-DRIVERS. More...
 

Function Documentation

§ Board_init()

void Board_init ( void  )

Performs "early" board-level initialization required by TI-DRIVERS.

Board_init() must be called before any other TI-DRIVER API. This function calls all device and board specific initialization functions needed by TI-DRIVERS; e.g., to initialize clocks and power management functionality.

This function should only be called once and as early in the application's startup as possible. In most applications, a call to Board_init() is the first statement in main().

Precondition
Board_init must be called after every CPU reset and prior to enabling any interrupts.
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale