63 #ifndef ti_drivers_aescmac_AESCMACLPF3__include 64 #define ti_drivers_aescmac_AESCMACLPF3__include 73 #include <ti/devices/DeviceFamily.h> 74 #include DeviceFamily_constructPath(inc/hw_types.h) 75 #include DeviceFamily_constructPath(driverlib/aes.h) 87 #if DeviceFamily_PARENT == DeviceFamily_PARENT_CC23X0 88 #define AESCMACLPF3_DEFAULT_AUTOCFG \ 89 ((uint32_t)AES_AUTOCFG_AESSRC_TXTXBUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3 | (uint32_t)AES_AUTOCFG_BUSHALT_EN) 90 #elif DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX 91 #define AESCMACLPF3_DEFAULT_AUTOCFG \ 92 ((uint32_t)AES_AUTOCFG_ECBSRC_TXTXBUF | (uint32_t)AES_AUTOCFG_TRGECB_WRBUF3 | (uint32_t)AES_AUTOCFG_BUSHALT_EN) 94 #error "Unsupported DeviceFamily_Parent for AESCMACLPF3!" 102 #if DeviceFamily_PARENT == DeviceFamily_PARENT_CC23X0 103 #define AESCMACLPF3_DMA_CONFIG ((uint32_t)AES_DMA_ADRCHA_BUF0 | (uint32_t)AES_DMA_TRGCHA_AESSTART) 104 #elif DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX 105 #define AESCMACLPF3_DMA_CONFIG ((uint32_t)AES_DMA_ADRCHA_BUF0 | (uint32_t)AES_DMA_TRGCHA_ECBSTART) 107 #error "Unsupported DeviceFamily_Parent for AESCMACLPF3!" 110 #define AESCBCMACLPF3_DMA_CONFIG AESCMACLPF3_DMA_CONFIG 129 volatile uint32_t intermediateTag[AES_TAG_LENGTH_BYTES / 4U];
130 uint32_t finalInputBlock[AES_BLOCK_SIZE_WORDS];
136 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) 162 void AESCMACLPF3_processBlocks(
const uint8_t *input,
size_t transactionLength);
171 void AESCMACLPF3_readTag(uint32_t tagOut[AES_TAG_LENGTH_BYTES / 4U]);
189 __STATIC_INLINE
bool AESCMAC_acquireLock(
AESCMAC_Handle handle, uint32_t timeout)
217 __STATIC_INLINE
void AESCMAC_enableThreadSafety(
AESCMAC_Handle handle)
220 object->threadSafe =
true;
235 __STATIC_INLINE
void AESCMAC_disableThreadSafety(
AESCMAC_Handle handle)
238 object->threadSafe =
false;
uint32_t tempAssetID
Definition: AESCMACLPF3.h:144
bool CryptoResourceLPF3_acquireLock(uint32_t timeout)
AES Global configuration.
Definition: AESCommon.h:154
AESCMACLPF3 Object.
Definition: AESCMACLPF3.h:125
AESCMAC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCMAC.h:771
AESCommonLPF3_Object common
Definition: AESCMACLPF3.h:128
bool segmentedOperationInProgress
Definition: AESCMACLPF3.h:148
void(* AESCMAC_CallbackFxn)(AESCMAC_Handle handle, int_fast16_t returnValue, AESCMAC_Operation *operation, AESCMAC_OperationType operationType)
The definition of a callback function used by the AESCMAC driver when used in AESCMAC_RETURN_BEHAVIOR...
Definition: AESCMAC.h:795
AESCMAC_OperationType operationType
Definition: AESCMACLPF3.h:133
AESCMAC_Operation * operation
Definition: AESCMACLPF3.h:132
AESCMAC_OperationalMode
Defines the operation modes for the AESCMAC driver.
Definition: AESCMAC.h:708
size_t inputLength
Definition: AESCMACLPF3.h:137
uint32_t keyAssetID
Definition: AESCMACLPF3.h:145
AESCMAC_CallbackFxn callbackFxn
Definition: AESCMACLPF3.h:131
AESCommonLPF3 Hardware Attributes.
Definition: AESCommonLPF3.h:80
void CryptoResourceLPF3_releaseLock(void)
AESCommon driver implementation for the Low Power F3 family.
bool threadSafe
Definition: AESCMACLPF3.h:135
Shared resources to arbitrate access to the AES engine.
int_fast16_t hsmStatus
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
Definition: AESCMACLPF3.h:143
AESCommonLPF3_HWAttrs AESCMACLPF3_HWAttrs
AESCMACLPF3 Hardware Attributes.
Definition: AESCMACLPF3.h:118
AESCMAC (CMAC and CBC-MAC) driver header.
void * object
Definition: AESCommon.h:157
Struct containing the parameters required for signing or verifying a message.
Definition: AESCMAC.h:717
AESCMAC_OperationalMode operationalMode
Definition: AESCMACLPF3.h:134
AESCommonLPF3 Object.
Definition: AESCommonLPF3.h:102