Instance: LRFDS2R
Component: LRFDS2R
Base address: 0x40085000
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4008 5000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4008 5004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4008 5008 |
|
RO |
32 |
0x0FFF 0000 |
0x0000 000C |
0x4008 500C |
|
WO |
32 |
0x0000 0000 |
0x0000 0010 |
0x4008 5010 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4008 5000 | Instance | 0x4008 5000 |
Description | Sample2RAM Config Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 | |||||||||||||||||
5 | LAST0 | When this bit is enabled, then the S2R will write all zeros, whenever it tries to write the stop address (instead of the regular value)
|
RW | 0 | |||||||||||||||||
4:3 | TRIGMODE | Trigger mode
|
RW | 0b00 | |||||||||||||||||
2:1 | SEL | Select sample source
|
RW | 0b00 | |||||||||||||||||
0 | CTL | Sample2RAM module enable
|
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4008 5004 | Instance | 0x4008 5004 |
Description | Sample2RAM Start Address Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:13 | RESERVED13 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 | |||||||||||
12:0 | ADDR | Memory start address for where to dump the samples. The address is word oriented starting from the start of the MCERAM, then RFERAM, then PBERAM, then S2RRAM and then BUFRAM. Also note that S2R has write priority to the RAMs, so any attempt at simultaneously accessing the RAMs used by S2R while it is running may be unreliable (no arbitration/stall implemented), and should be avoided. 0 -> 1023 : MCERAM 1024 -> 2047 : RFERAM 2048 -> 3071 : PBERAM 3072 -> 4095 : S2RRAM 4096 -> 4479 : BUFRAM
|
RW | 0b0 0000 0000 0000 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4008 5008 | Instance | 0x4008 5008 |
Description | Sample2RAM Stop Address Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:13 | RESERVED13 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 | |||||||||||
12:0 | ADDR | Memory start address for where to dump the samples. The address is word oriented starting from the start of the MCERAM, then RFERAM, then PBERAM, then S2RRAM and then BUFRAM. Also note that S2R has write priority to the RAMs, so any attempt at simultaneously accessing the RAMs used by S2R while it is running may be unreliable (no arbitration/stall implemented), and should be avoided. 0 -> 1023 : MCERAM 1024 -> 2047 : RFERAM 2048 -> 3071 : PBERAM 3072 -> 4095 : S2RRAM 4096 -> 4479 : BUFRAM
|
RW | 0b0 0000 0000 0000 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x4008 500C | Instance | 0x4008 500C |
Description | Sample2RAM Status Register | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:28 | RESERVED28 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | |||||||||||
27:16 | ADDRCNT | Current address counter value
|
RO | 0xFFF | |||||||||||
15:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | |||||||||||
0 | RUNNING | S2R running status
|
RO | 0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x4008 5010 | Instance | 0x4008 5010 |
Description | Sample2RAM Trigger Register | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
0 | TRIG | Trigger a new sample capture (or arm it if the trigger mode is trigger on event)
|
WO | 0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |