Flash Layout for On-Chip OAD¶
This section will describe the method for placing images in internal flash when using on-chip OAD.
Constraints and Requirements for On-chip OAD (stack library)¶
The following points must be considered for On-chip OAD applications:
The user application must be sufficiently small in order to fit into the flash layout system described below
User app functionality is lost while performing OAD (Persistent app is running)
Internal Flash Memory Layout¶
The internal flash of the device contains the active user application, the user application’s stack, the persistent application, the persistent application’s stack, and the secure bootloader. Each application’s role is defined below.
Note
As we have assumed the stack-library approach, the stack images referenced below are a part of each application image (i.e. the user and persistent apps have their own dedicated stack)
Application Name |
Description |
MCUboot bootloader |
|
Persistent application |
|
Stack (2) |
|
User application |
|
![../_images/ditaa-9eb071e583f421cbedbda9744819be25b1dd5f31.png](../_images/ditaa-9eb071e583f421cbedbda9744819be25b1dd5f31.png)
Note
Based on different devices, the address of each component listed above might
vary. The address used in the persistent application linker file
should match the settings in the flash_map_backend.h
file.
#define BOOTLOADER_BASE_ADDRESS 0x00000000
#define BOOT_BOOTLOADER_SIZE 0x00006000
#define BOOT_PRIMARY_1_BASE_ADDRESS 0x00006000
#define BOOT_PRIMARY_1_SIZE 0x00076000
#define BOOT_SECONDARY_1_BASE_ADDRESS 0x00043000
#define BOOT_SECONDARY_1_SIZE 0x0003d000