CC2340R5 to CC2340R22 Porting Guide¶
This section will describe, in general terms, how to migrate a project developed for the CC2340R5 device to a CC2340R22 device running the SimpleLink Low Power F3 SDK. However, it is important to first assess the differences between both devices to make sure that the project migration is possible (See Platform Devices Comparison).
Evaluate the CC2340R22 device when only having CC2340R5 devices¶
To evaluate the CC2340R22 when only having a CC2340R5, you can modify the Flash size as described bellow:
Open the Linker command file
.cmdand modify the Flash size to 256 kB.1#define FLASH_SIZE 0x40000
Note
The two devices are API compatible, a project for CC2340R22 developed on CC2340R5 can be migrated (via the migration guide below) with very few modifications to be built and flashed on CC2340R22.
Migration Guide¶
The recommended migration path is to start with a CC2340R5 based example project from the SimpleLink Low Power F3 SDK and follow the next steps:
Import the project into Code Composer Studio or you IDE of preference.
Open SysConfig, go to
Device Viewand click onSWITCH.
Figure 195. SysConfig - Switch Device.¶
Once the
Switch Board or Devicewindow is opened, select the CC2340R22 board, or CC2340R22 device and click onCONFIRM. Make sure to save the project changes so that the migration takes place.
Figure 196. SysConfig - Select CC2340R22 device.¶
Build the project.
Additional Steps for Off-Chip OAD and MCUBoot examples¶
Note
The CC2340R22 device does not support On-Chip and Dual Image OAD due to reduced Flash size.
Right click on the project file and select Properties. Modify the post build steps so that the slot sizes match the ones of the CC2340R22 device.
Figure 197. Project Properties - Modify post build steps.¶
Import MCUBoot project, modify the
flash_map_backend.hadding the following lines of code. In addition, addDeviceFamily_CC23X0R22as part of thePredefined Symbolsof the project (right click on Properties → Predefined Symbols).1 #elif defined DeviceFamily_CC23X0R22 2 #define BOOTLOADER_BASE_ADDRESS 0x00000000 3 #define BOOT_BOOTLOADER_SIZE 0x00006000 4 5 #define BOOT_PRIMARY_1_BASE_ADDRESS 0x00006000 6 #define BOOT_PRIMARY_1_SIZE 0x00036000 7 8 #define BOOT_SECONDARY_1_BASE_ADDRESS 0x00023000 9 #define BOOT_SECONDARY_1_SIZE 0x00036000
To finish with the MCUBoot project, go inside
mcuboot_configand do the following:- Uncomment the following two lines:
- Listing 171. mcuboot_config.h - Uncomment to enable external flash configuration and enable the overwrite-only code path.¶
1 #define TI_BOOT_USE_EXTERNAL_FLASH 2 #define MCUBOOT_OVERWRITE_ONLY
- Comment out the following line:
1 //#define MCUBOOT_DIRECT_XIP
Build both projects.