Radio Control Layer (RCL)
|
#include <stdint.h>
#include <ti/drivers/utils/List.h>
Go to the source code of this file.
Data Structures | |
struct | RCL_Buffer_TxBuffer |
Definition of an RCL Tx Buffer. More... | |
struct | RCL_Buffer_DataEntry |
Definition of an RCL Rx Buffer Entry. More... | |
struct | RCL_MultiBuffer |
Definition of an RCL Rx MultiBuffer. More... | |
struct | RCL_MultiBuffer_ListInfo |
Information about an RCL_MultiBuffer list being traversed. More... | |
Macros | |
#define | RCL_Buffer_bytesToWords(byteLen) (((byteLen) + sizeof(uint32_t) - 1) / sizeof(uint32_t)) |
Number of 32-bit words needed to hold a given number of bytes (rounded up) More... | |
#define | RCL_Buffer_DataEntry_paddedLen(len) (RCL_Buffer_bytesToWords((len) + sizeof(uint16_t)) * sizeof(uint32_t)) |
Total length of a data entry in bytes based on length field of the entry. More... | |
#define | RCL_Buffer_entryLen(numPad, hdrLen, dataLen) (RCL_Buffer_DataEntry_paddedLen(sizeof(uint8_t) + (numPad) + (hdrLen) + (dataLen))) |
Total length of a data entry in bytes, including entry length field and padding. More... | |
#define | RCL_TxBuffer_len(numPad, hdrLen, dataLen) (offsetof(RCL_Buffer_TxBuffer, length) + RCL_Buffer_entryLen(numPad, hdrLen, dataLen)) |
Total length of a TX buffer in bytes, including all fields and padding. More... | |
#define | RCL_TxBuffer_len_u32(numPad, hdrLen, dataLen) (RCL_Buffer_bytesToWords(RCL_TxBuffer_len(numPad, hdrLen, dataLen))) |
Total length of a TX buffer in 32-bit words, including all fields and padding. More... | |
#define | RCL_MultiBuffer_len(dataLen) (offsetof(RCL_MultiBuffer, data) + (dataLen)) |
Total length of a multi buffer in bytes, including all fields. More... | |
#define | RCL_MultiBuffer_len_u32(dataLen) (RCL_Buffer_bytesToWords(RCL_MultiBuffer_len(dataLen))) |
Total length of a multi buffer in 32-bit words, including all fields. More... | |
Enumerations | |
enum | RCL_BufferState { RCL_BufferStatePending = 0U, RCL_BufferStateInUse = 1U, RCL_BufferStateFinished = 2U } |
Buffer state. More... | |
Functions | |
static RCL_Buffer_TxBuffer * | RCL_TxBuffer_get (List_List *list) |
Function to atomically get the first elem in a Tx Buffer list. More... | |
static RCL_Buffer_TxBuffer * | RCL_TxBuffer_head (List_List *list) |
Function to return the head of a TxBuffer list. More... | |
static RCL_Buffer_TxBuffer * | RCL_TxBuffer_next (RCL_Buffer_TxBuffer *elem) |
Function to return the next elem in a linked list of Tx Buffers. More... | |
uint8_t * | RCL_TxBuffer_init (RCL_Buffer_TxBuffer *buffer, uint32_t numPad, uint32_t hdrLen, uint32_t dataLen) |
Function to initialize a TX buffer entry for use by RCL. More... | |
void | RCL_TxBuffer_put (List_List *list, RCL_Buffer_TxBuffer *elem) |
Function to atomically put an elem onto the end of a Tx Buffer list. More... | |
static RCL_MultiBuffer * | RCL_MultiBuffer_head (List_List *list) |
Function to return the head of a MultiBuffer list. More... | |
static RCL_MultiBuffer * | RCL_MultiBuffer_next (RCL_MultiBuffer *elem) |
Function to return the next elem in a linked list of MultiBuffers. More... | |
static RCL_MultiBuffer * | RCL_MultiBuffer_get (List_List *list) |
Function to get the first elem in a MultiBuffer list. More... | |
void | RCL_MultiBuffer_clear (RCL_MultiBuffer *buffer) |
Function to clear a multi buffer entry for re-use by RCL. More... | |
void | RCL_MultiBuffer_init (RCL_MultiBuffer *buffer, size_t size) |
Function to initialize a multi buffer entry for use by RCL. More... | |
RCL_Buffer_DataEntry * | RCL_MultiBuffer_RxEntry_get (List_List *list, List_List *consumedBuffers) |
Function to get the first entry in a MultiBuffer list. More... | |
bool | RCL_MultiBuffer_RxEntry_isEmpty (List_List *list) |
Function to check if the MultiBuffer List is out of entries. More... | |
void | RCL_MultiBuffer_ListInfo_init (RCL_MultiBuffer_ListInfo *listInfo, List_List *list) |
Function to initialize information for traversing a multi buffer list. More... | |
RCL_Buffer_DataEntry * | RCL_MultiBuffer_RxEntry_next (RCL_MultiBuffer_ListInfo *listInfo) |
Function to return the next entry in a list of multi buffers. More... | |
bool | RCL_MultiBuffer_RxEntry_isLast (RCL_MultiBuffer_ListInfo *listInfo) |
Function to check a traversed entry was the last one. More... | |
void | RCL_MultiBuffer_put (List_List *list, RCL_MultiBuffer *elem) |
Function to atomically put an elem onto the end of a multi buffer list. More... | |
RCL_MultiBuffer * | RCL_MultiBuffer_findFirstWritableBuffer (RCL_MultiBuffer *head) |
Find the first writable buffer in a list of MultiBuffers. More... | |
RCL_MultiBuffer * | RCL_MultiBuffer_getBuffer (RCL_MultiBuffer *curBuffer, uint32_t minLength) |
Returns a buffer with at least minLength bytes remaining capacity. More... | |
uint32_t | RCL_MultiBuffer_findAvailableRxSpace (const RCL_MultiBuffer *curBuffer) |
Find the minumum number of bytes that can be stored in available MultiBuffers. More... | |
static uint8_t * | RCL_MultiBuffer_getNextWritableByte (RCL_MultiBuffer *curBuffer) |
Find the first byte to write in an RCL_MultiBuffer. More... | |
static void | RCL_MultiBuffer_commitBytes (RCL_MultiBuffer *curBuffer, uint32_t numBytes) |
Update number of bytes written to RCL_MultiBuffer. More... | |
struct RCL_MultiBuffer_s |
Definition of an RCL Rx MultiBuffer.
Instances of RCL_MultiBuffer are allocated by the protocol stacks, and provided to RCL
Data Fields | ||
---|---|---|
List_Elem | __elem__ | |
RCL_BufferState | state |
Buffer state |
uint16_t | length |
Number of bytes in the data field |
uint16_t | headIndex |
Number of bytes consumed |
uint16_t | tailIndex |
Number of bytes written |
uint8_t | data[] |
Data buffer consisting of RCL_Buffer_DataEntry elements |
struct RCL_MultiBuffer_ListInfo_s |
Information about an RCL_MultiBuffer list being traversed.
An instance of RCL_MultiBuffer_ListInfo is used to hold information of an RX queue which is read without consuming directly.
Data Fields | ||
---|---|---|
List_List * | multiBuffers |
Pointer to list of MultiBuffers |
RCL_MultiBuffer * | nextBuffer |
Pointer to next MultiBuffer to traverse |
uint16_t | nextIndex |
Index of nextBuffer->data for next entry |
#define RCL_Buffer_bytesToWords | ( | byteLen | ) | (((byteLen) + sizeof(uint32_t) - 1) / sizeof(uint32_t)) |
Number of 32-bit words needed to hold a given number of bytes (rounded up)
Referenced by RCL_Handler_BLE5_dtmTx().
#define RCL_Buffer_DataEntry_paddedLen | ( | len | ) | (RCL_Buffer_bytesToWords((len) + sizeof(uint16_t)) * sizeof(uint32_t)) |
Total length of a data entry in bytes based on length field of the entry.
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_aux_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_BLE5_updateTxBuffers(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_updateTxBuffers(), RCL_Handler_Nesb_Prx(), RCL_Handler_Nesb_Ptx(), RCL_MultiBuffer_RxEntry_get(), and RCL_MultiBuffer_RxEntry_next().
enum RCL_BufferState |