Radio Control Layer (RCL)
|
#include <stdint.h>
#include <stdlib.h>
#include <ti/drivers/rcl/RCL_Command.h>
#include <ti/drivers/rcl/RCL_Debug.h>
#include <ti/drivers/rcl/LRF.h>
#include <ti/log/Log.h>
Functions | |
LRF_SetupResult | LRF_loadImage (const LRF_TOPsmImage *image, uint32_t destinationAddress) |
void | LRF_initSettingsState (LRF_ApplySettingsState *state, LRF_ApplySettingsBase includeBase, uint16_t phyFeatures) |
LRF_SetupResult | LRF_applySettings (LRF_ConfigWord *config, LRF_ApplySettingsState *state, int32_t bufferAvailWords) |
LRF_TxPowerTable_Entry | LRF_TxPowerTable_findValue (const LRF_TxPowerTable *table, LRF_TxPowerTable_Index powerLevel) |
Search for settings corresponding to the highest tx power lower than specified value in the tx power table. More... | |
LRF_SetupResult LRF_loadImage | ( | const LRF_TOPsmImage * | image, |
uint32_t | destinationAddress | ||
) |
References SetupResult_ErrorImageLen, SetupResult_Ok, and TOPSM_RAM_SZ.
Referenced by LRF_setupRadio().
void LRF_initSettingsState | ( | LRF_ApplySettingsState * | state, |
LRF_ApplySettingsBase | includeBase, | ||
uint16_t | phyFeatures | ||
) |
References LRF_ApplySettingsState::includeBase, LRF_resetSettingsState(), and LRF_ApplySettingsState::phyFeatures.
Referenced by LRF_resetSettingsState(), and LRF_setupRadio().
LRF_SetupResult LRF_applySettings | ( | LRF_ConfigWord * | config, |
LRF_ApplySettingsState * | state, | ||
int32_t | bufferAvailWords | ||
) |
References HW_Region_Clear, HW_Write_16bit, HW_Write_16bit_masked, HW_Write_16bit_sparse, HW_Write_32bit, LRF_ApplySettingsState::includeBase, LRF_BASE_ADDR, LRF_RegionOperation_Invalid, LRF_RegionOperation_Skip, LRF_ConfigWord::masked, MAX_REG_CONFIG_LEN, Par_Reference_32bit, Par_Region_Clear, Par_Write_32bit, PBE_RAM_BASE_ADDR, LRF_ApplySettingsState::phyFeatures, RCL_Debug_assert, LRF_ConfigWord::region, LRF_ConfigWord::segment, SetupResult_ErrorConfigLen, SetupResult_ErrorElemAddrAlign, SetupResult_ErrorElemLen, SetupResult_ErrorElemType, SetupResult_ErrorParRange, SetupResult_Ok, SetupResult_Ok_Partial, LRF_ConfigWord::sparse, SW_Region_Clear, SW_Write_16bit, SW_Write_16bit_sparse, SW_Write_32bit, swParamList, swParamListSz, LRF_ConfigWord::value16, and LRF_ConfigWord::value32.
Referenced by LRF_resetSettingsState(), and LRF_setupRadio().
LRF_TxPowerTable_Entry LRF_TxPowerTable_findValue | ( | const LRF_TxPowerTable * | table, |
LRF_TxPowerTable_Index | powerLevel | ||
) |
Search for settings corresponding to the highest tx power lower than specified value in the tx power table.
table | pointer to the tx power table to be searched |
powerLevel | maximum allowed power level |
References LRF_getRawTxPower(), LRF_TxPower_Use_Max, LRF_TxPower_Use_Min, LRF_TxPower_Use_Raw, LRF_TxPowerEntry_INVALID_VALUE, LRF_TxPowerTable::numEntries, LRF_TxPowerTable_Entry::power, LRF_TxPowerTable::powerTable, and LRF_TxPowerTable_Index::rawValue.
Referenced by LRF_programTxPower(), and LRF_resetSettingsState().