Data Fields
EventP_Struct Union Reference

EventP structure. More...

#include <EventP.h>

Data Fields

uint32_t dummy
 
uint8_t data [(52)]
 

Detailed Description

EventP structure.

Opaque structure that should be large enough to hold any of the RTOS specific EventP objects.

Field Documentation

§ dummy

uint32_t EventP_Struct::dummy

Align object

§ data

uint8_t EventP_Struct::data[(52)]

The documentation for this union was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale