![]() |
![]() |
Structure for MCAN Tx FIFO/Queue Status. More...
#include <MCAN.h>
Data Fields | |
uint32_t | freeLvl |
uint32_t | getIdx |
uint32_t | putIdx |
uint32_t | fifoFull |
Structure for MCAN Tx FIFO/Queue Status.
uint32_t MCAN_TxFIFOQStatus::freeLvl |
Tx FIFO Free Level
uint32_t MCAN_TxFIFOQStatus::getIdx |
Tx FIFO Get Index Read as zero when Tx Queue operation is configured.
uint32_t MCAN_TxFIFOQStatus::putIdx |
Tx FIFO/Queue Put Index
uint32_t MCAN_TxFIFOQStatus::fifoFull |
Tx FIFO/Queue Full 0 = Tx FIFO/Queue not full 1 = Tx FIFO/Queue full