LGPTimerLPF3 channel dependent pin configuration struct. More...
#include <LGPTimerLPF3.h>
Data Fields | |
uint8_t | pin |
uint8_t | pinMux |
uint8_t | nPin |
uint8_t | nPinMux |
LGPTimerLPF3 channel dependent pin configuration struct.
LGPTimer struct used by the LGPTimerLPF3_HWAttrs.
uint8_t LGPTimerLPF3_ChannelConf::pin |
Channel pin
uint8_t LGPTimerLPF3_ChannelConf::pinMux |
Channel pin mux
uint8_t LGPTimerLPF3_ChannelConf::nPin |
Complementary channel pin
uint8_t LGPTimerLPF3_ChannelConf::nPinMux |
Complementary channel pin mux