Data Fields
BatMonSupportLPF3_Config Struct Reference

BatMon Support Configuration. More...

#include <BatMonSupportLPF3.h>

Data Fields

uint32_t intNum
 
uint32_t intPriority
 
uint32_t intMux
 

Detailed Description

BatMon Support Configuration.

A sample structure is shown below:

const BatMonSupportLPF3_Config BatMonSupportLPF3_config = {
.intNum = INT_CPUIRQ2,
.intPriority = (~0),
.intMux = EVTSVT_CPUIRQ2SEL_PUBID_AON_PMU_COMB,
};

Field Documentation

§ intNum

uint32_t BatMonSupportLPF3_Config::intNum

Device-specific interrupt number

§ intPriority

uint32_t BatMonSupportLPF3_Config::intPriority

Device-specific interrupt priority

§ intMux

uint32_t BatMonSupportLPF3_Config::intMux

Device-specific interrupt muxing


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale