ECDH software driver implementation for the Low Power F3 family.
============================================================================
This file should only be included in the board file to fill the ECDH_config struct.
The driver is backed by a software ECC library implementation.
The driver implementation supports the following curves for ECDH:
Curves Supported |
---|
NISTP256 |
Curve25519 |
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ECDH.h>
#include <third_party/ecc/include/lowlevelapi.h>
Go to the source code of this file.
Data Structures | |
struct | ECDHLPF3SW_HWAttrs |
ECDHLPF3SW Hardware Attributes. More... | |
struct | ECDHLPF3SW_Object |
ECDHLPF3SW Object. More... | |
Macros | |
#define | ECDHLPF3SW_ECC_WINDOW_SIZE 3 |
#define | ECDHLPF3SW_ECC_WORKZONE_WORDS 198 |
#define ECDHLPF3SW_ECC_WINDOW_SIZE 3 |
#define ECDHLPF3SW_ECC_WORKZONE_WORDS 198 |