Data Structures | Macros | Typedefs
AESCTRLPF3.h File Reference

Detailed Description

AESCTR driver implementation for the Low Power F3 family.

==========================================================================

Hardware Accelerator

The Low Power F3 family of devices has a dedicated AES hardware that can perform AES encryption operations with 128-bit keys. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set.

Implementation Limitations

Runtime Parameter Validation

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.

#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/AESCTR.h>
#include <ti/drivers/cryptoutils/aes/AESCommonLPF3.h>
#include <ti/drivers/cryptoutils/sharedresources/CryptoResourceLPF3.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/aes.h)>
Include dependency graph for AESCTRLPF3.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESCTRLPF3_Object
 AESCTRLPF3 Object. More...
 

Macros

#define AES_AUTOCFG_CTRENDN_BIGENDIAN   AES_AUTOCFG_CTRENDIAN_BIGENDIAN
 
#define AESCTRLPF3_DEFAULT_AUTOCFG
 
#define AESCTRLPF3_LAST_BLOCK_AUTOCFG
 

Typedefs

typedef AESCommonLPF3_HWAttrs AESCTRLPF3_HWAttrs
 AESCTRLPF3 Hardware Attributes. More...
 

Macro Definition Documentation

§ AES_AUTOCFG_CTRENDN_BIGENDIAN

#define AES_AUTOCFG_CTRENDN_BIGENDIAN   AES_AUTOCFG_CTRENDIAN_BIGENDIAN

§ AESCTRLPF3_DEFAULT_AUTOCFG

#define AESCTRLPF3_DEFAULT_AUTOCFG
Value:
((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | \
(uint32_t)AES_AUTOCFG_TRGAES_RDTXT3 | (uint32_t)AES_AUTOCFG_CTRSIZE_CTR128 | \
(uint32_t)AES_AUTOCFG_CTRENDN_BIGENDIAN | (uint32_t)AES_AUTOCFG_BUSHALT_EN)
#define AES_AUTOCFG_CTRENDN_BIGENDIAN
Definition: AESCTRLPF3.h:82

§ AESCTRLPF3_LAST_BLOCK_AUTOCFG

#define AESCTRLPF3_LAST_BLOCK_AUTOCFG
Value:
((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | \
(uint32_t)AES_AUTOCFG_CTRSIZE_CTR128 | (uint32_t)AES_AUTOCFG_CTRENDN_BIGENDIAN | \
(uint32_t)AES_AUTOCFG_BUSHALT_EN)
#define AES_AUTOCFG_CTRENDN_BIGENDIAN
Definition: AESCTRLPF3.h:82

Typedef Documentation

§ AESCTRLPF3_HWAttrs

AESCTRLPF3 Hardware Attributes.

AESCTRLPF3 hardware attributes should be included in the board file and pointed to by the AESCTR_config struct.

© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale